CubeMars: Doubling Torque with Half the Weight - Unveiling Our Advantages

Randy / Aug 07,2023

We are excited to share an intriguing discovery about CubeMars motors and how they outperform the competition. Recently, one of our colleagues received an email from a customer, drawing attention to a significant difference between our R80 KV110 Outrunner Torque Motor and a comparable product from a leading rival.


customer's email


Upon closer examination of the catalog, we were thrilled to find that despite being nearly the same size (90mm in diameter x ~27.5mm in length), our R80 KV110 motor weighs almost half as much as our competitor's. What excited us even more was the revelation that our R80 Torque Motor offers nearly double the continuous torque compared to our rival's product.


Cubemars R80 motor compared with similar products


Naturally, we were intrigued by this remarkable difference, especially considering the reputation of our competitor. Seeking clarity, we reached out to the hardware engineer at CubeMars's factory, and here's what we discovered:


Advantages of CubeMars R80 motor


The secret lies in our core advantage – an extremely high fill rate achieved through our meticulous hand-winding method. Additionally, the CubeMars R80 Outrunner Torque Motor boasts a greater number of pole pairs, coupled with the use of premium coil materials and superior magnets that set new standards in the market.


Core advantages of CubeMars R80 motor


In today's fast-paced manufacturing landscape, brushless DC motor manufacturers and industries at large strive for high productivity through automated processes. However, an excessive reliance on fully autonomous production may overlook potential issues, resulting in compromised performance.


At CubeMars, we recognize the value of a balanced approach.


CubeMars factory


We understand that some customers may wonder why our delivery times, especially for custom products, can be longer than expected.


The reason is simple: we are committed to maintaining the highest quality standards.

To achieve this, we meticulously perform core processes manually, which may cause slight delays in delivery.


At CubeMars, our focus is not only on meeting your needs but surpassing your expectations. We pride ourselves on delivering motors that offer unmatched performance, reliability, and longevity. With our hand-wound craftsmanship and attention to detail, we ensure that every motor leaving our factory is a testament to our unwavering commitment to quality.


CubeMars Team


Related Articles
Daniel Simu's Robot Takes the Stage on America's Got Talent with Power from CubeMars AK Series Motors
Daniel Simu's Robot Takes the Stage on America's Got Talent with Power from CubeMars AK Series Motors
In the upcoming episode of America's Got Talent, viewers will witness a unique performance as artist Daniel Simu takes the stage with his specially designed robot for an enchanting dance routine. This captivating performance wouldn't be possible without t
May 14,2024
CubeMars Motors Empower Michaël’s Team to Develop an Autonomous Stretching Device
CubeMars Motors Empower Michaël’s Team to Develop an Autonomous Stretching Device
Michaël, who suffers from muscular dystrophy, used his own experiences to collaborate with his team to develop an innovative calf stretching device. This device, equipped with CubeMars motors, provides a more convenient rehabilitation treatment option for
Dec 27,2024
CubeMars Shines at the 2nd China Conference on Humanoid Robotics and Embodied Intelligence
CubeMars Shines at the 2nd China Conference on Humanoid Robotics and Embodied Intelligence
CubeMars debuts AKH hollow planetary module at the 2nd China Humanoid Robotics Conference, winning Outstanding Supplier and showcasing cutting-edge innovation.
Jun 04,2025
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt