Cubemars - 17 Year Motor Manufacturer info@cubemars.com +86 13755649079
English
English
中文简体
日本語
Deutsch
Français
한국어
Español
Pусский
Quick Registration
Create your CubeMars account

 

Moment
TABLE OF CONTENTS
The Driver Board
The Encoder
The Hall Sensor

Meeting Diverse Needs: CubeMars' Customized Electronic Solutions for Motor Products

CubeMars / May 22,2024

At CubeMars, we provide tailored solutions to complement our BLDC motors, meeting the diverse needs of customers in the robotics and automation industry. This includes offering a driver board for the AK series, an encoder for the GL gimbal motor, and a hall sensor for the RI and RO motors. What are the fundamental principles behind these complementary components, and why did CubeMars decide to integrate them into various motors?


The Driver Board


A motor driver, also known as a driver board or motor controller, is essential for efficient motor control. Here's a breakdown:


1.Direction and Speed Control: They enable precise control over motor direction and speed by adjusting power supply or modulation techniques like PWM accordingly.


2.Protection Features: Motor drivers include safeguards such as overcurrent, overvoltage, thermal shutdown, and short-circuit protection to prevent damage to the motor and driver.


3.Interface Compatibility: Designed to work with various motor types and communication protocols like PWM, UART, or CAN, they ensure seamless integration with different systems.


4.Integration with Control Systems: Motor drivers are often part of larger control systems in robotics, CNC machines, or industrial automation setups, working alongside sensors and microcontrollers for precise motor control.


The Driver Board


In summary, motor drivers are vital for translating control signals into precise motor movements, ensuring efficient and reliable operation across diverse applications. 


Our CubeMars Driver Board, the second iteration of planetary brushless motor controllers seamlessly integrated into the AK series, offers unparalleled performance and versatility. With an onboard encoder and built-in temperature sensor, it ensures precision and reliability while providing overload and over-temperature protection.


The Encoder


An encoder measures the position, speed, or direction of rotation of a motor shaft or other moving parts. It typically consists of a sensor that detects changes in position and generates electrical signals corresponding to those changes. Encoders offer precise control and feedback in various applications, including robotics, CNC machines, and servo motors. 


CubeMars utilizes a magnetic rotary encoder with a 14-bit high-resolution output, ensuring maximum system accuracy, particularly crucial for gimbal motors that require higher precision.


The Hall Sensor

The Hall Sensor


Hall sensors detect the presence of a magnetic field and provide a digital output signal indicating its presence or absence. They are commonly used in BLDC motors to determine rotor position for commutation. While providing limited positional accuracy compared to encoders, Hall sensors are cost-effective and simple. 


CubeMars' Hall sensors, integrated into the RO and RI series frameless torque motor, enable real-time monitoring of motor temperature and provide precise rotor position and speed information, ensuring optimal motor control.


At CubeMars, our fundamental philosophy revolves around prioritizing quality in all our endeavors. We are driven by a singular mission: to continuously innovate and develop, so that we can consistently deliver products that not only meet but exceed our clients' exacting standards.


Join hands with CubeMars, and together, let us shape a future defined by stability and reliability in the realm of robot power systems.


Related Articles
How to Improve Exoskeleton Responsiveness and Adaptability: Powered by CubeMars AK80-64
How to Improve Exoskeleton Responsiveness and Adaptability: Powered by CubeMars AK80-64
Tunable-stiffness knee exoskeleton improving adaptability, response speed, and gait stability in rehabilitation robotics powered by CubeMars AK80-64
May 20,2026
CubeMars' AK70-10 Powering the Future of Agile Robotics
CubeMars' AK70-10 Powering the Future of Agile Robotics
At CubeMars, we are excited to be part of cutting-edge innovation in robotics!Last year, our AK70-10 BLDC motors were integral to the success of Nathan Weiss's groundbreaking bipedal robot project at Stellenbosch University, South Africa.
Oct 29,2024
Gorilla Mk1 Robot: Powered by CubeMars Motors, Paving the Way for New Heights in Overhead Line Maintenance
Gorilla Mk1 Robot: Powered by CubeMars Motors, Paving the Way for New Heights in Overhead Line Maintenance
In the realm of overhead line maintenance in Australia, a pioneering robot developed by Crest Robotics is transforming work practices.
Oct 31,2024
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt