DC Motors 
Stepper Motors
Servo Motors
Brushless DC Motors (BLDC)
Actuators
Linear Motors

What motor used in robots

CubeMars / Oct 26,2023

Robots use various types of motors, depending on their specific applications and requirements. Some of the most common types of motors used in robots include:


DC Motors 


Direct current (DC) motors are commonly used in robotics due to their simplicity and ease of control. They are often used in wheeled robots for propulsion. DC motors can be controlled using voltage and polarity changes to adjust speed and direction.


Stepper Motors


Stepper motors are known for their precision in controlling position and rotation. They are often used in applications where precise control is required, such as 3D printers and CNC machines.


Servo Motors


Servo motors provide precise control over the position and speed of the robot's components. They are commonly used in robotic arms and other applications that demand accuracy.


Brushless DC Motors (BLDC)


BLDC motors are known for their high efficiency and reliability. They are often used in applications where long-term continuous operation is required, such as drones, electric vehicles, and industrial robots.


Actuators


In some robotic applications, specialized actuators are used, such as pneumatic or hydraulic actuators. These can provide high force output and are commonly used in heavy-duty industrial robots.


Linear Motors


Linear motors are used in applications where linear motion is required. They are often seen in high-precision, high-speed robotic systems, including pick-and-place machines and linear stages.


The choice of motor depends on the specific needs of the robot's tasks, such as speed, accuracy, torque, and environmental conditions. Additionally, control systems and algorithms are tailored to the chosen motor type to achieve the desired performance. It's important to carefully select the right motor type for the robot's intended application to ensure optimal functionality.


Related Articles
CubeMars Empowers the University of Minnesota’s Agricultural Quadruped Robot: Highly Integrated Motors Drive Smart Farming
CubeMars Empowers the University of Minnesota’s Agricultural Quadruped Robot: Highly Integrated Motors Drive Smart Farmi...
The agricultural quadruped robot dog navigates fields, collects data, and performs tasks that traditional wheeled robots and drones cannot handle on complex terrain.
Jun 10,2025
How to Choose the Right Robot Joint Motor: Torque, Speed & Integration Explained
How to Choose the Right Robot Joint Motor: Torque, Speed & Integration Explained
Learn how to select the right robot joint motor by analyzing torque requirements, speed, and precision to ensure stable, efficient, and reliable robotic motion.
Feb 10,2026
Introducing the Revolutionary RI-PH Series of Sealed Frameless Motors from CubeMars
Introducing the Revolutionary RI-PH Series of Sealed Frameless Motors from CubeMars
In the realm of robotics and industrial automation, the performance and reliability of motors are of paramount importance. CubeMars is proud to announce the launch of its latest RI-PH series of sealed frameless motors, designed to deliver outstanding elec
Aug 01,2024
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt