Why Do Motors Determine Robot Dog Performance?
Core Parameters of Robot Dog Motors
In-Depth Case Study of Robot Dog Motors
University of Minnesota Agricultural Quadruped Robot – Stability and Reliability in Practice
KLEIYN – Vertical Climbing Quadruped Robot Pushing Limits
Kemba – Precision-Driven Robot
Bottom-Line Logic for Robot Dog Motor Selection – Derived from Case Studies
Robot Dog Motor Product Recommendations and Selection Advice
Conclusion

Which Parameters Matter for Quadruped Robot Motors? From “Able to Move” to “High-Performance Motion”

CubeMars / Apr 14,2026

From "Able to Move" to "High-Performance Motion": How Motors Are Redefining Quadruped Robots

 

Over the past few years, quadruped robots (robot dogs) have undergone a significant technological transition:

 

  • From "able to walk" → to "stable walking"

  • From "basic motion" → to "high-speed dynamic running"

  • From "research prototype" → to "industrial-grade deployment (inspection / security / rescue)"

 

Throughout this process, one key trend has become increasingly clear:

 

The core of robotic performance competition is shifting from "algorithmic capability" to "actuation system capability."

 

Early robot development relied more on:

 

  • Gait planning

  • Control algorithms (PID / MPC)

  • Perception systems (vision / IMU)

 

However, as technology has advanced, the industry has gradually recognized a practical reality:

 

No matter how advanced the algorithm, without sufficiently powerful, fast, and precise actuators, high-performance motion cannot be achieved.

 

In other words:

 

  • Algorithms determine "how the robot wants to move"

  • Motors determine "whether it can actually do so"

 

Therefore, a core question now faces engineers:

 

  • How to select a motor truly suitable for a robot dog?

  • Which parameters are critical?

  • How to balance performance and cost?

 

Why Do Motors Determine Robot Dog Performance?

 

Many people believe that a robot dog's "intelligence" comes primarily from algorithms.

 

But in real engineering, a more practical conclusion is:

 

The performance ceiling of a robot dog is often determined by the motor (actuator), not the algorithm.

 

I.  Algorithms Only Provide Decisions; Motors Provide Execution

 

A simple analogy:

 

  • Algorithm → Brain (decides how to move)

  • Motor → Muscle (actually executes the movement)

 

If the "muscle" is not strong enough, fast enough, or precise enough:

 

  • No matter how good the algorithm, it cannot be realized

  • Ideal motions cannot be achieved

 

For example:

 

  • The algorithm commands a jump → insufficient motor torque → cannot jump

  • The algorithm requires rapid adjustment → slow response → the robot has already lost balance

 

Motor capability directly limits the algorithm's potential.

 

II.  All Motion Is Essentially Motor Operation

 

Every action of a robot dog depends on the actuators:

 

  • Lifting a leg → motor outputs torque

  • Landing → motor absorbs impact

  • Balancing → motor continuously makes fine adjustments

  • Running → motor responds at high speed

 

In other words:

When a robot "appears to move," it is essentially the motor continuously outputting control results.

 

III. Actuator = Power + Control + Perception

 

Modern robot dogs do not use a "bare motor" but an integrated actuator, typically including:

 

  • Motor (power)

  • Gearbox (torque amplification)

  • Encoder (position feedback)

  • Driver (control execution)

 

This means:

The motor itself is already part of the control system.

 

What are the implications?

 

  • Control precision → affects stability

  • Response speed → affects dynamic capability

  • Torque output → affects load capacity

 

Actuator performance = Robot motion quality

 

IV.  Motor Parameters Directly Determine Motion Performance

 

Different parameters correspond to different capabilities:

 

  • Torque → can it "hold up"?

  • Peak torque → can it "explode"?

  • Response speed → can it "keep up"?

  • Control precision → can it "stay steady"?

 

If any of these is insufficient:

 

  • The robot will shake

  • It will respond sluggishly

  • Or it will be unable to perform complex motions

 

V.  Why Are High-Performance Robots Upgrading Their Actuators?

 

A clear trend in the industry in recent years is:

 

Shifting from algorithm optimization → to actuator system upgrades

 

The reason is simple:

 

  • Algorithms can optimize "strategy"

  • Actuators determine "physical capability"

 

In summary:

Algorithms determine what the robot wants to do, while motors determine how well it can do it.

 

Core Parameters of Robot Dog Motors

 

1.  Rated Torque – "Sustained Combat Capability"

 

Definition: The continuous output capability of the motor under long-term stable operation (Nm)

 

Why is it critical?

 

  • Determines whether the robot can "stand"

  • Determines whether it can operate for extended periods

  • Directly affects load capacity

 

Engineering conclusion: Rated torque = lower limit of basic performance

 

2.  Peak Torque – "Instantaneous Burst Power"

 

Definition: The maximum output capability of the motor over a short period

 

Typical applications:

 

  • Jumping

  • Climbing

  • Emergency posture adjustment

 

Peak torque determines limit motion capability

 

Note:

 

  • Cannot be used continuously

  • Typically 2–3 times the rated torque

 

3.  Gear Ratio – "Balancing Speed and Power"

 

Core relationship:

 

  • Higher gear ratio → higher torque / lower speed

  • Lower gear ratio → higher speed / more responsive

 

Selection logic:

 

  • Dynamic robots → low gear ratio

  • Heavy-load robots → high gear ratio

 

Essentially a trade-off between power and flexibility

 

4.  Control Accuracy – "Core of Stability"

 

Key metrics:

 

  • Encoder precision (14bit / 16bit+)

  • Torque control accuracy

 

Impact:

 

  • Whether the robot shakes

  • Whether it can perform fine motions

  • Whether it can achieve biomimetic gaits

 

High accuracy = high stability

 

5.  Response Speed – "Key to Running Capability"

 

Definition: Delay from control signal to motion execution

 

Impact:

 

  • Dynamic balance

  • Gait switching

  • Obstacle avoidance capability

 

The faster the response, the "smarter" the robot

 

6.  Torque Density – "Core Metric for Lightweighting"

 

Definition: Output capability per unit weight (Nm/kg)

 

Significance:

 

  • Lighter → more agile

  • Lighter → more energy-efficient

  • Lighter → longer endurance

 

One of the core metrics for high-end robots

 

7.  Voltage & Power

 

Common:

 

  • 24V: Lightweight applications

  • 48V: Industrial grade

 

Trend:

 

High-performance robots are gradually migrating to 48V systems (higher efficiency)

 

8.  Level of Integration (Integrated Actuator)

 

An integrated actuator includes:

 

  • Motor + driver + encoder + gearbox

 

Advantages:

 

  • Reduces development complexity

  • Improves reliability

  • Shortens development cycle

 

Current mainstream trend in the industry

 

In-Depth Case Study of Robot Dog Motors


University of Minnesota Agricultural Quadruped Robot – Stability and Reliability in Practice


omni-agrobot-2

 

Project Background

The quadruped robot (OmniAgRobot) from the University of Minnesota Agricultural Robotics Lab is used for:

 

  • Field inspection

  • Crop health monitoring

  • Soil data collection

 

This robot can move freely in cornfields, muddy terrain, and irregular terrain – something traditional wheeled robots struggle to achieve.

 

Why a Quadruped Structure?

 

Compared to wheeled robots or drones:

 

  • Muddy ground → wheeled robots easily get stuck

  • Between crop rows → wheeled robots cannot enter

  • Irregular terrain → insufficient stability

 

Quadruped robots offer:

 

  • Greater terrainability

  • Higher stability

  • More precise path control

 

Motor Selection: The Key Role of the AK70-10

 

The project ultimately chose the AK70-10 integrated actuator for the following core reasons:

 

① High Integration

 

  • Motor + gearbox + driver integrated

  • Simplifies mechanical structure and wiring

  • Improves system reliability

 

② High-Precision Control

 

  • Supports CAN communication

  • Supports multi-motor synchronization

  • Enables complex gait coordination

 

③ High Torque Output

 

  • Adapts to muddy ground, slopes, and other complex environments

  • Provides stable support

 

④ High Reliability and Ease of Deployment

 

  • Easy to install

  • Efficient debugging

  • Shortens development cycle

 

Actual Engineering Performance

 

During testing, the robot achieved:

 

  • Synchronized coordination of multiple motors

  • High-frequency position and torque control

  • Stable walking in complex terrain

 

Research team feedback:

High integration + high torque significantly improved system stability and development efficiency

 

Core Conclusion

The core requirements for agricultural robots are not "extreme performance" but:

 

  • Stability

  • Reliability

  • Sustainable operation

 

Essential needs:

 

Medium-high torque + high precision + high reliability

 

KLEIYN – Vertical Climbing Quadruped Robot Pushing Limits

 

kleiyn-climbing

 

Project Highlights:

 

  • Can climb between narrow walls of 800–1000mm

  • Motion speed increased approximately 50-fold

  • Adapts to complex environments (e.g., chimneys/shafts)

 

Motor Configuration Breakdown

 

ComponentActuator ModelCore PerformanceRole
Leg ActuatorAK70-10 KV100Strong continuous support, high torque densityProvides stable support and continuous motion, suitable for walking and dynamic movement
Waist ActuatorAK10-9 V2.0 KV60Peak torque up to 48Nm, high burst outputProvides core burst power for posture adjustment and high-dynamic actions

 

Why Can It Climb?

 

Three key factors:

 

1. High rated torque

  • Ensures continuous adhesion without falling

 

2. High peak torque

  • Provides burst power for leg lifting and propulsion

 

3. Low-latency response

  • Quickly adjusts contact points (prevents slipping / loss of balance)

 

Engineering conclusion:

 

Extreme motion = Torque + Response + Control, all three combined

 

Kemba – Precision-Driven Robot


Kemba

 

Project Characteristics

 

  • High-precision gait control

  • Strong force control capability

  • Used for research and control algorithm validation

 

Motor Capability Requirements

 

  • Precise foot placement control

  • Torque variation control (compliance control)

  • High-bandwidth response

 

Engineering Significance

In research robots:

 

  • High torque ≠ good performance

  • Controllability is the core

 

Core Conclusion

 

Future robot trend = Precision-driven + Force control integration

 

Bottom-Line Logic for Robot Dog Motor Selection – Derived from Case Studies

 

After understanding the core parameters and real-world cases, the most critical next step is:

 

Selecting the actuator solution that truly fits your project.

 

From the three typical cases – KLEIYN, the agricultural robot, and Kemba – we can identify a crucial pattern:


Different application scenarios correspond to fundamentally different "motor parameter combination strategies."

 

No single parameter is the strongest; the key is the right combination.

 

I.  Extreme Motion Scenario (KLEIYN)

 

Keywords: Dynamic capability / Burst power / Response speed

 

Core needs:

 

  • High peak torque (burst)

  • High response speed (rapid adjustment)

  • Medium-high rated torque (sustained support)

 

Why?

 

  • Climbing, jumping, and fast movement all require substantial instantaneous power

  • Simultaneously, rapid adjustment is essential to avoid losing balance

 

Essential logic:

 

Prioritize "response + burst," then sustained capability

 

II.  Agricultural / Industrial Scenario (University of Minnesota Robot)

 

Keywords: Stability / Reliability / Continuous operation

 

Core needs:

 

  • Stable rated torque

  • High reliability (long operation hours)

  • High integration (reduces system complexity)

 

Why?

 

  • Farm environments are complex but the pace is relatively slow

  • Requires long-duration operation, not extreme performance

 

Essential logic:

 

Prioritize "stability + reliability," not extreme performance

 

III. Research / Control Scenario (Kemba)

 

Keywords: Precision / Force control / Repeatability

 

Core needs:

 

  • High-precision encoder

  • Fine torque control

  • High-bandwidth control system

 

Why?

 

  • Need to validate algorithms

  • Need repeatable experimental results

 

Essential logic:

 

Prioritize "controllability," not just raw power

 

Comparison of the Three Scenario Types

 

Scenario TypeRepresentative CasePriority OrderCore Motor Metrics
Extreme MotionKLEIYNResponse > Peak torque > Rated torqueDynamic performance
Agricultural/IndustrialUniversity of MinnesotaRated torque > Reliability > IntegrationStability
Research ControlKembaControl precision > Force control > ResponseControllability


Robot Dog Motor Product Recommendations and Selection Advice

 

Application ScenarioTypical UseCore NeedsRecommended ModelReason
Dynamic Robot DogHigh-speed quadruped / jumping / climbingHigh response + medium-high torque + low latencyAK70-10 KV100Excellent dynamic performance, balanced torque and response, suitable for running, jumping, and complex motions
Agricultural / Industrial RobotField inspection / pipeline inspectionStability + reliability + long-duration operationAK70-10 KV100 / AK80-8 KV60High rated torque + high integration, supports long-term stable operation
Heavy-Load RobotMaterial handling / Industrial equipmentHigh torque + high load capacityAK80-9 V3.0 KV100High rated torque + high integration, supports long-term stable operation
Research / Education ProjectLab work / control algorithm developmentFlexibility + cost control + ease of developmentAK60-6 V3.0 KV80Compact size, easy integration, suitable for rapid prototyping and development


Quick Decision Guide

 

Your GoalRecommended Model
Run fast / Strong dynamicsAK70-10 KV100
Stable and reliable operationAK70-10 KV100 / AK80-8 KV60
High torque / Heavy load capacityAK80-9 V3.0 KV100
Rapid development / TeachingAK60-6 V3.0 KV80

 

Conclusion

 

The transition of quadruped robots from “able to move” to “high-performance motion” is no longer driven by algorithms, but by motor actuators. Algorithms determine how a robot “wants to move,” while motors determine how well it “can perform.” Modern integrated actuators are themselves the core of the control system, directly defining the performance ceiling of quadruped robots.

 

Different application scenarios correspond to completely different motor parameter combination strategies. Extreme motion scenarios prioritize response speed and peak torque, agricultural and industrial scenarios prioritize rated torque and reliability, while research and education scenarios prioritize control accuracy and force control capability. There is no “strongest” motor—only the most suitable parameter configuration.

 

Motor selection is not a competition of a single parameter, but a system-level balance among torque, response, precision, weight, and cost. Dynamic quadruped robots focus on response and burst power, industrial and agricultural scenarios emphasize stability and continuous operation, heavy-load applications require high torque reserves, and research and education place greater importance on controllability and ease of development.

 

The key to advancing quadruped robots from “able to move” to “high-performance motion” is not how powerful the algorithm is, but whether the motor can support, keep up, and control accurately. Only by choosing the right motor can a quadruped robot truly run fast, stand stable, and perform precise tasks.

Related Articles
CubeMars Motors Empower Michaël’s Team to Develop an Autonomous Stretching Device
CubeMars Motors Empower Michaël’s Team to Develop an Autonomous Stretching Device
Michaël, who suffers from muscular dystrophy, used his own experiences to collaborate with his team to develop an innovative calf stretching device. This device, equipped with CubeMars motors, provides a more convenient rehabilitation treatment option for
Dec 27,2024
CubeMars Exhibits at the 2024 World Robot Conference
CubeMars Exhibits at the 2024 World Robot Conference
August 23, 2024, Beijing—At the 2024 World Robot Conference, CubeMars took center stage as an exhibitor, presenting its full range of motor products and drawing significant attention from attendees. The event brought together leading experts, investors, a
Aug 28,2024
Do robots use AC or DC Motors?
Do robots use AC or DC Motors?
Robots can use both AC (alternating current) and DC (direct current) motors, depending on their specific applications and requirements. Each type of motor has its advantages and is chosen based on the particular needs of the robot's tasks.
Oct 16,2023
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt