Chimney Climbing: A New Era for Quadruped Robots
The Core of KLEIYN’s Legs with AK70-10 (Max Torque 24.8 Nm)
Strong Core with AK10-9 V2.0 KV60 Robotic Actuator (Max Torque 48 Nm)
Why This Matters: From Labs to Real-World Applications
CubeMars Redefines Vertical Mobility

Robot Dog Climbs Walls with Robotic Actuators,50 Times Fater!

CubeMars / Sep 02,2025

Robot Dogs Beyond Flat Ground

The age of the robot dog is rapidly advancing. Once limited to walking and running on flat terrain, today’s quadruped robots are tackling extreme environments—from rough ground to vertical shafts. One of the most striking breakthroughs is KLEIYN, a chimney-climbing quadruped robot designed with an active waist joint and powered by CubeMars robotic actuators.


kleiyn-climbing.jpg


Unlike traditional robot dogs that struggle in confined spaces, KLEIYN can press its legs and torso against two walls and climb vertically, much like a human rock climber.



Chimney Climbing: A New Era for Quadruped Robots


KLEIYN weighs around 18 kg, measures 760 mm in body length, and offers 13 degrees of freedom (3 DOF per leg + 1 waist DOF). Its unique design allows the robot to wedge itself between walls spaced 800–1000 mm apart and ascend at speeds up to 150 mm/s—around 50× faster than earlier attempts at vertical climbing robots.


robot-dog-climbs-wall


This innovation comes from the waist joint motor, which lets the robot flex its torso, adapt to wall spacing, and maintain stability during vertical movement. The result is a chimney climbing robot dog that transitions seamlessly between ground locomotion and vertical ascent.


The Core of KLEIYN’s Legs with AK70-10 (Max Torque 24.8 Nm)


waist-design.jpg


The robot’s legs are equipped with CubeMars AK70-10 actuators, delivering up to 24.8 Nm torque. These compact yet powerful motors provide: AK70-10 KV100 Robotic Actuator


● Fast reflexes and low latency, critical for quick foot placement and wall adjustments;

● High torque output, enabling stable pressure against vertical surfaces;

● Quasi-direct drive smoothness, reducing vibration and ensuring fluid climbing cycles.


With AK70-10 KV100 robotic actuator in each leg joint, KLEIYN can perform rapid micro-adjustments to adapt to uneven wall surfaces while maintaining continuous upward force.


kleiyn-joint.jpg


Strong Core with AK10-9 V2.0 KV60 Robotic Actuator (Max Torque 48 Nm)


The true innovation lies in the waist joint, powered by CubeMars AK10-9 V2.0 KV60 actuator. Much like a human climber’s core muscles, this joint is the central stabilizer during chimney climbing. 


● 48 Nm torque capacity—double that of the leg actuators—provides the strength to brace the torso between two walls;

● Sustained stability, keeping the robot securely wedged even under dynamic leg movements;

● Dynamic posture control, thanks to low-latency response for bending and extending in sync with climbing cycles;

● Mechanical “core strength” effect, ensuring the torso channels power efficiently without drift or instability.


With AK10-9 V2.0 KV60, the waist becomes more than a connector—it is the key to vertical climbing stability, transforming KLEIYN into a reliable climbing quadruped robot.


Why This Matters: From Labs to Real-World Applications

 

The combination of robot dog agility and waist joint stability opens up a wide range of possibilities:


● Search and Rescue: climbing through collapsed buildings, vertical shafts, or narrow debris zones;

● Industrial Inspection: accessing chimneys, ventilation ducts, and confined pipelines;

● Exploration: navigating caves, fissures, and geological formations beyond human reach.

With CubeMars robotic actuators, KLEIYN shows how quadruped robots with waist joints can go where no robot dog has gone before.


CubeMars Redefines Vertical Mobility


KLEIYN demonstrates the next leap for quadruped robot dogs—climbing walls instead of being confined to the ground. Powered by CubeMars AK70-10 KV100 robotic actuators for nimble leg control and the AK10-9 robotic actuator for a strong, stabilizing waist joint, the robot achieves smooth, powerful, and reliable chimney climbing.


CubeMars continues to lead the way in robotics with high-torque, low-latency, quasi-direct drive actuators, enabling breakthroughs in mobility, agility, and adaptability.


CubeMars robotic actuators: where robot dogs gain the strength to climb.


Related Articles
The Journey of Humanoid Robots
The Journey of Humanoid Robots
The exploration of humanoid robots has spanned nearly a century, from the rudimentary Herbert Televox by Westinghouse in 1927 to the advanced "Prime Mover" by Tesla today. This journey reflects humanity's fascination with the creator's identity and its ul
Oct 20,2023
How to Choose Underwater Thrusters: Guide for ROV and AUV Propulsion Systems
How to Choose Underwater Thrusters: Guide for ROV and AUV Propulsion Systems
Learn how to choose the right underwater thruster for ROV and AUV systems based on efficiency, control, reliability, and mission requirements.
May 27,2026
How to Choose the Right Robot Joint Motor: Torque, Speed & Integration Explained
How to Choose the Right Robot Joint Motor: Torque, Speed & Integration Explained
Learn how to select the right robot joint motor by analyzing torque requirements, speed, and precision to ensure stable, efficient, and reliable robotic motion.
Feb 10,2026
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt