Cubemars - 17 Year Motor Manufacturer info@cubemars.com +86 13755649079
English
English
中文简体
日本語
Deutsch
Français
한국어
Español
Pусский
Quick Registration
Create your CubeMars account

 

Moment
TABLE OF CONTENTS
1. Why BLDC Motor Driver Selection Matters in Robotics
2. Why Is FOC Widely Used in Robot Motors
3. How Feedback Methods Affect BLDC Motor Driver Selection
4. How FOC Works with Different Feedback Methods
5. How to Determine Whether a BLDC Motor and Drive Are Compatible
6. How to Choose a BLDC Motor Driver for Different Robotic Applications
7. Key Parameters to Check When Choosing a Drive
8. Common BLDC Motor Driver Selection Mistakes
9. Conclusion: How to Choose the Right BLDC Motor Driver for Robotics
FAQ: Frequently Asked Questions

How to Choose a BLDC Motor Driver for Robotics: A Guide to FOC Control and Feedback Selection

CubeMars / Nov 05,2026

1. Why BLDC Motor Driver Selection Matters in Robotics


Brushless DC (BLDC) motors offer high power density, good efficiency, and a long service life. They are widely used in humanoid robots, quadruped robots, robotic arms, exoskeletons, and industrial automation equipment.

 

However, motor performance alone does not determine the overall performance of a system. The motor driver controls the motor's current, speed, and torque, and adjusts its operating state based on feedback signals. The driver's control strategy, feedback method, and parameter configuration all affect the motor's response speed, operating stability, control accuracy, and dynamic performance.

 

For example, joint motors in humanoid and quadruped robots need to start and stop frequently, reverse direction quickly, and adjust output torque in real time according to movement conditions. Exoskeleton motors, on the other hand, place greater emphasis on smooth motion, torque adjustment, and safety during human-machine interaction. These applications place high demands on motor driver control capabilities.

 

When selecting a BLDC motor driver, the following factors should be considered:

 

  • Control strategy: Does the driver support Field-Oriented Control (FOC), and can it meet the application's torque and dynamic control requirements?

  • Position feedback: Choose Hall sensors, encoders, or sensorless control based on the required control accuracy and operating conditions.

  • Control modes: Does the driver support torque, speed, and position control?

  • Electrical parameters: Are the voltage, current, speed, and torque ratings compatible with the motor?

  • System compatibility: Do the feedback interfaces, communication methods, and protection functions meet the application requirements?

 

Understanding how these factors work together helps you choose the right BLDC motor drive solution for robot motors.

 

2. Why Is FOC Widely Used in Robot Motors

 

Field-Oriented Control (FOC) is a motor control method that regulates the magnetic field and electromagnetic torque by controlling the stator current vector.

 

FOC transforms the motor's three-phase currents into a rotating reference frame and independently controls the torque-producing current and magnetizing current, allowing the motor current to be adjusted more precisely according to control commands.

 

Compared with traditional six-step commutation, FOC generally provides smoother torque output and improves low-speed performance and dynamic response. As a result, it is widely used in robot joint motors and servo drive systems.

 

2.1 Key Features of FOC

 

Smoother Torque Output

 

By regulating the current vector, FOC controls the motor's electromagnetic torque and helps reduce torque ripple, resulting in smoother motor operation. This is particularly important for robot joints that require continuous and precise movement.

 

Good Low-Speed Performance

 

Robot joints often need to operate at low speeds while maintaining stable torque output. FOC can improve low-speed performance through precise current control. However, the actual results also depend on the position feedback method, control algorithm, and motor parameters.

 

Fast Dynamic Response

 

During robot movement, motors may need to accelerate, decelerate, and reverse direction frequently. FOC can quickly adjust motor output through the current loop, supporting dynamic torque control.

 

Support for Multiple Motion Control Modes

 

FOC can serve as the underlying current control method for torque, speed, and position control. The specific modes supported depend on the driver's control architecture and firmware configuration.

 

2.2 What Are the Requirements of FOC for Position Feedback and Current Sensing?

 

FOC requires not only motor current control but also the acquisition or estimation of rotor position to perform coordinate transformations and current regulation correctly.

 

Therefore, an FOC motor driver typically needs the following capabilities:

 

  • Current sensing: Measures the motor phase currents through current sampling to provide data for current loop control.

  • Rotor position feedback: Obtains rotor position information through Hall sensors, encoders, or sensorless algorithms.

  • Current loop control: Adjusts the driver's output based on the difference between the target current and the actual current.

  • Parameter configuration: Configures the control system according to motor parameters such as pole pairs, resistance, inductance, and feedback devices.

 

Current sensing accuracy, sampling timing, and position feedback quality all affect the actual control performance of FOC.

 

2.3 Which Robotics Applications Are Suitable for FOC?


ApplicationMain Control RequirementsBenefits of FOC
Humanoid RobotsJoint torque control and fast responseImproves dynamic torque regulation
Quadruped RobotsFrequent starts and stops, forward and reverse rotation, and low-speed movementImproves motion smoothness
Exoskeleton DevicesSmooth output and torque adjustmentSupports precise joint control
Robotic ArmsPosition accuracy, speed control, and torque controlSupports precise motion control
Custom Robot JointsLimited installation space and varying dynamic loadsProvides flexible control solutions

 

It is important to note that FOC does not automatically mean that a system provides high-precision position control or full servo functionality. Actual performance must also be evaluated based on the feedback devices, control loops, driver hardware, and mechanical transmission structure.

 

3. How Feedback Methods Affect BLDC Motor Driver Selection

 

In addition to the control strategy, rotor position feedback is another important factor when selecting a BLDC motor driver.

 

The driver needs to obtain or estimate the rotor position to control the motor current and operating state correctly. Common methods include Hall sensor feedback, encoder feedback, and sensorless control.

 

It is important to distinguish between these methods: Hall sensors and encoders are physical position feedback devices, while sensorless control estimates rotor position using motor operating signals. All three methods can be used to obtain position information in a motor control system, but they differ in feedback accuracy, low-speed performance, and system cost.


Related Article:Sensorless vs. Encoder-Based BLDC Motor Control in Robotics

 

3.1 Hall Sensor

 

Hall sensors detect changes in the rotor's magnetic field to provide rotor position and commutation signals. A typical three-Hall sensor configuration provides information about six position sectors within one electrical cycle.

 

Key characteristics:

 

  • Simple structure and relatively low cost.

  • Provides basic position feedback at low speeds and during startup.

  • Suitable for applications that do not require high position resolution.

  • Relatively limited position resolution, making it difficult to meet high-precision position control requirements on its own.

 

Hall sensors can be used not only for conventional commutation control but also with certain FOC drives that support Hall-based position feedback. However, due to their limited feedback resolution, their control accuracy and low-speed performance are generally inferior to those of high-resolution encoder-based solutions.

 

3.2 Encoder

 

Encoders provide more precise rotor position feedback and are commonly used in motor systems that require high control accuracy and dynamic response.

 

Based on their operating principles, common encoders can be divided into the following types:

 

  • Incremental encoders: Determine relative position by outputting and counting pulses. A reference position usually needs to be established at startup.

  • Absolute encoders: Directly provide absolute angular position within a single revolution. Some models also support multi-turn position tracking.

 

Key characteristics:

 

  • Provide high-resolution position feedback.

  • Help achieve precise speed, torque, and position control.

  • Suitable for robot joints, robotic arms, and servo systems.

  • Require attention to resolution, signal interfaces, communication protocols, and drive compatibility.

 

Common encoder interfaces include ABZ incremental signals and digital interfaces such as SPI, SSI, and BiSS. Encoder interfaces are not necessarily universal across different drives, so specific compatibility should be confirmed before selection.

 

For robot joints equipped with gearboxes, it is also important to distinguish between a motor-side encoder and an output-side joint encoder. Gearbox backlash, transmission errors, and structural flexibility may affect output position accuracy. Some applications may therefore require additional output-side position feedback.

 

3.3 Sensorless Control

 

Sensorless control does not rely on physical position sensors such as Hall sensors or encoders. Instead, it estimates rotor position or speed using electrical signals such as back EMF, current, and voltage.

 

Key characteristics:

 

  • No additional rotor position sensor is required.

  • Helps reduce sensor-related hardware costs and installation space.

  • Can simplify the mechanical structure of certain motor systems.

  • Sensitive to algorithms, parameter configuration, and operating conditions.

  • Conventional back-EMF-based sensorless solutions have difficulty estimating rotor position at zero and extremely low speeds.

 

Sensorless control is commonly used in fans, pumps, and some equipment that does not require high torque control performance at low speeds.

 

For applications such as robot joints that require frequent starts and stops, low-speed operation, and stable torque output, the actual performance of sensorless algorithms during startup, low-speed operation, and load changes should be carefully evaluated. Some advanced algorithms can improve position estimation at low or zero speeds through techniques such as high-frequency injection, but both the motor and the drive must support these methods.

 

3.4 Comparison of Different Feedback Methods


Comparison ItemHall SensorEncoderSensorless Control
Physical Position SensorRequiredRequiredNot required
Position ResolutionLowHighDepends on the estimation algorithm
Zero-Speed StartupProvides initial position informationProvides position feedbackDepends on the estimation method
Low-Speed OperationGenerally usable, but with limited accuracyGenerally performs wellLimitations with conventional back-EMF-based solutions
Control AccuracyModerateHighDepends on the algorithm and operating conditions
System CostLowRelatively highCan reduce sensor hardware requirements
Typical ApplicationsGeneral motor controlRobot joints and servo systemsFans, pumps, and similar equipment


4. How FOC Works with Different Feedback Methods

 

FOC and position feedback methods belong to different technical layers. FOC determines how the drive controls motor current, while Hall sensors, encoders, and sensorless control determine how the drive obtains or estimates rotor position.

 

Different feedback methods can be combined with FOC, but actual support depends on the drive's hardware design and control algorithms.

 

4.1 Combining FOC with Different Feedback Methods


Feedback MethodCombination with FOCKey CharacteristicsSuitable Applications
Hall SensorSensored FOCProvides basic rotor position feedback with simple hardwareMotor systems that do not require high position resolution
EncoderSensored FOCHigher-resolution position feedback and stronger control capabilitiesRobot joints, robotic arms, and servo systems
Sensorless ControlSensorless FOCNo additional position sensor required; relies on algorithm-based estimationApplications with relatively low requirements for low-speed and zero-speed control

 

FOC + encoder is a common combination in robot joints and precision motion control systems. It provides high-resolution position feedback for torque, speed, and position control.

 

FOC + Hall sensor can meet the needs of some applications with relatively moderate cost and control accuracy requirements.

 

Sensorless FOC can reduce the need for position sensor hardware, but its performance during zero-speed startup and low-speed operation should be verified based on the specific algorithm.

 

4.2 Comparison of Feedback Solutions for Different Robotic Applications


ApplicationMain Control RequirementsFeedback Options to Consider
Humanoid Robot JointsHigh dynamic response, low-speed stability, and torque controlEncoder
Quadruped Robot JointsFast response, frequent forward and reverse rotation, and torque controlEncoder
Exoskeleton DevicesSmooth operation, torque adjustment, and low-speed controlEncoder
Robotic ArmsPosition accuracy, speed control, and smooth motionEncoder
General Rotary Drive EquipmentBasic speed control and cost managementHall sensor or sensorless control

 

These are common selection guidelines rather than fixed configurations. The actual choice should also take into account the motor type, drive compatibility, control accuracy, and operating conditions.

 

5. How to Determine Whether a BLDC Motor and Drive Are Compatible

 

After determining the FOC control strategy and feedback method, you also need to check the electrical parameters, control capabilities, and interface compatibility between the robot motor and the drive.

 

5.1 Are the Voltage and Current Ratings Compatible?

 

First, confirm that the operating voltage ranges of the motor and drive are compatible. Then check whether the drive's continuous and peak current ratings meet the motor's operating requirements.

 

Key points to consider:

 

  • Motor rated voltage and drive input voltage range.

  • Motor rated current and drive continuous output current.

  • Motor peak current and drive peak output capability.

  • Maximum allowable peak current duration.

  • Overcurrent and overvoltage protection provided by the power supply and drive.

 

Note that peak current can usually only be supplied for a short period under specified time limits and cooling conditions. It should not be treated as equivalent to continuous output capability.

 

5.2 Do the Speed and Torque Meet the Application Requirements?

 

The drive must have sufficient current and voltage control capabilities to meet the motor's operating requirements under different speed and load conditions.

 

During selection, consider the motor's rated speed, maximum speed, rated torque, and peak torque, as well as load inertia, acceleration time, and the actual operating cycle.

 

For robot joints, in addition to peak torque, pay attention to continuous torque and torque stability during low-speed operation.

 

5.3 Is the Feedback Method Compatible?

 

If Hall sensors or encoders are used, confirm that the drive supports the corresponding feedback devices and signal interfaces.

 

For example:

 

  • Hall sensor signal type and phase configuration.

  • Incremental or absolute encoder type.

  • Encoder resolution and communication protocol.

  • Motor pole pairs and position feedback parameters.

  • Encoder installation direction and electrical angle offset.

 

Incompatible feedback interfaces may prevent the motor from starting properly or achieving the expected control accuracy.

 

5.4 Does the Drive Support the Required Control Modes?

 

Different applications have different requirements for drive control modes. Common modes include:


Control ModeMain FunctionTypical Applications
Speed ControlControls the motor to reach the target speedRotary drive equipment
Torque ControlControls the motor's output torque or torque-producing currentRobot joints and force-controlled actuators
Position ControlControls the motor to reach a specified angle or positionRobotic arms and positioning platforms

 

FOC can serve as the underlying current control strategy for torque, speed, and position control. However, the specific modes supported depend on the drive's control architecture and firmware.

 

For robotic applications, also check whether the drive supports stable low-speed operation, zero-speed holding, and rapid forward and reverse rotation.

 

5.5 Do the Communication Interfaces and Protection Functions Meet the Requirements?

 

For multi-motor robotic systems, the drive must also provide suitable communication interfaces and protection functions.

 

Common communication methods include CAN, UART, and RS485. Some high-performance motion control systems also use real-time industrial communication protocols such as EtherCAT.

 

During selection, confirm the following:

 

  • Whether the drive supports the communication protocol required by the system.

  • Whether it meets the update frequency requirements for control commands and feedback data.

  • Whether it supports coordinated control of multiple motors.

  • Whether it provides overcurrent, overvoltage, undervoltage, and overtemperature protection.

  • Whether its cooling and installation requirements can be met by the application.

 

For robotic systems involving frequent deceleration or externally driven motor operation, also consider the DC bus voltage rise caused by regenerative energy and the braking energy handling capabilities of the drive and power supply system.

 

6. How to Choose a BLDC Motor Driver for Different Robotic Applications

 

Different robotic applications have different requirements for motor drives. Selection should take into account the motor's joint structure, load characteristics, operating speed, control accuracy, and system integration method.

 

6.1 Humanoid and Quadruped Robots

 

Humanoid and quadruped robots typically require multiple motors to work together to perform complex movements. Their joint motors need to handle frequent starts and stops, rapid responses, and bidirectional torque output.

 

Key factors to consider for these applications include:

 

  • High torque density and compact installation space.

  • Good low-speed operating stability.

  • Fast torque response and dynamic control capabilities.

  • Encoder feedback and position control capabilities.

  • Multi-joint communication and coordinated control capabilities.

 

For these applications, FOC with encoder feedback is worth considering. Depending on the joint structure, an integrated actuator or a quasi-direct-drive motor may be suitable.

 

For example, CubeMars AKE Series QDD motors combine a brushless motor with a planetary gearbox. They can be used in humanoid robot joints, exoskeletons, and compact robotic actuators. During selection, confirm the drive configuration, feedback method, gear ratio, and control interface of the specific model.

 

6.2 Collaborative Robots and Robotic Arms

 

Collaborative robots and robotic arms typically require high position control accuracy, smooth motion, and reliable repeatability.

 

Key factors to consider include:

 

  • Encoder feedback resolution.

  • Position and speed closed-loop control capabilities.

  • Low-speed operating stability.

  • Torque control and response to load changes.

  • Multi-axis communication and synchronization capabilities.

 

For joint systems that require compact integration, integrated robotic power modules may be worth considering.

 

CubeMars AK Series robotic actuators are an option for robotic joint applications. Their drive configuration, encoder, communication protocol, and control modes should be confirmed for each specific model.

 

6.3 Custom Robot Joints

 

In some robotic designs, the dimensions, mounting structure, or output performance of standard motors may not fully meet the requirements. In such cases, the motor may need to be integrated directly into the joint structure.

 

Frameless torque motors are suitable for this type of customized design.

 

Key factors to consider include:

 

  • Stator and rotor dimensions and mounting structure.

  • Rated torque and peak torque.

  • Motor cooling and continuous operating capability.

  • Encoder or Hall sensor configuration.

  • Parameter compatibility between the external drive and motor.

 

CubeMars RI frameless inrunner torque motors and RO frameless outrunner torque motors can be used in different robot joint designs. Since frameless motors typically require external drives and feedback systems, the motor, sensors, drive, and mechanical structure should be evaluated as an integrated system.

 

6.4 Industrial Automation Equipment

 

Industrial automation equipment typically requires stable speed control, reliable continuous operation, and good system compatibility.

 

For conveyor systems, automated mechanisms, and general rotary drive loads, an appropriate drive solution can be selected according to the required operating accuracy and cost considerations.

 

If the equipment requires high-precision positioning, multi-axis synchronization, or frequent starts and stops, give priority to FOC, encoder feedback, closed-loop control, and real-time communication capabilities.

 

6.5 Medical Rehabilitation and Inspection Robots

 

Medical rehabilitation equipment and inspection robot motors have high requirements for smooth operation, reliability, and control safety.

 

For example, exoskeleton devices need to adjust joint output torque according to human movement, while inspection robots may need to maintain stable operation across different terrains and load conditions.

 

These applications should be evaluated for low-speed performance, torque control capability, feedback reliability, temperature rise, and protection functions. The drive solution should also meet the specific safety requirements of the equipment.

 

7. Key Parameters to Check When Choosing a Drive

 

Before determining the drive model, it is recommended to organize the motor specifications and actual application requirements to avoid performance issues caused by parameter mismatches.


Parameter CategoryWhat to CheckPurpose
Motor TypeBLDC, motor structure, and back-EMF waveformDetermine compatibility with the drive control strategy
Operating VoltageRated voltage and operating voltage rangeConfirm power supply compatibility
Current CapabilityRated current, continuous current, peak current, and peak current durationConfirm drive capability
Speed and TorqueRated speed, maximum speed, rated torque, and peak torqueEvaluate load compatibility
Control StrategyFOC and specific control algorithmsMatch application requirements
Feedback MethodHall sensors, incremental encoders, absolute encoders, or sensorless controlMeet position feedback requirements
Control ModeTorque, speed, or position controlMatch motion control objectives
Communication InterfaceCAN, UART, RS485, etc.Meet system communication requirements
Operating EnvironmentOperating temperature, cooling conditions, and installation spaceEnsure reliable operation
Protection FunctionsOvercurrent, overvoltage, undervoltage, and overtemperature protectionImprove system reliability

  

If the application involves frequent deceleration, rapid direction changes, or high load inertia, also confirm whether the drive and power supply system support the required braking and regenerative energy handling solutions.

 

8. Common BLDC Motor Driver Selection Mistakes

 

In practice, some seemingly straightforward selection decisions can prevent a motor from achieving its expected performance.

 

Mistake 1: Focusing Only on the Drive's Peak Current

 

Peak current is not the same as continuous current. If continuous output capability, peak current duration, and cooling conditions are overlooked, the drive may overheat or shut down due to protection limits during extended operation.

 

Mistake 2: Assuming That an Encoder Always Means FOC

 

An encoder is a position feedback device, while FOC is a control strategy. They belong to different technical categories. Although encoders are commonly used in FOC systems, the control strategy used by a drive cannot be determined solely by whether it has an encoder.

 

Mistake 3: Assuming That Sensorless Control Is Suitable for All Low-Speed Applications

 

Conventional back-EMF-based sensorless control has difficulty estimating rotor position at zero and extremely low speeds. For robot joints that require stable low-speed torque and reliable zero-speed startup, sensorless solutions should be evaluated carefully.

 

Mistake 4: Overlooking Feedback Interface Compatibility Between the Motor and Drive

 

Even if the motor and drive have compatible voltage and current ratings, incompatible encoder protocols, Hall signals, or position parameters may prevent the system from operating properly.

 

Mistake 5: Focusing Only on Motor Peak Torque and Ignoring Continuous Operating Capability

 

Peak torque generally refers to the motor's short-term output capability. For robot joints that need to support loads over extended periods or operate frequently, continuous torque, temperature rise, and cooling conditions must also be considered.

 

Mistake 6: Ignoring the Actual Motion Requirements of the Application

 

Different devices have different requirements for speed, torque, position accuracy, and response time. Selecting a drive based only on motor power or rated speed can easily overlook the actual control requirements.

 

9. Conclusion: How to Choose the Right BLDC Motor Driver for Robotics

 

Choosing a BLDC motor driver requires considering the control strategy, position feedback method, electrical parameters, and actual application requirements together.

 

FOC enables precise torque adjustment by controlling the motor's current vector. It is generally suitable for robotic applications that require smooth operation, good low-speed performance, and fast dynamic response.

 

Regarding feedback methods, Hall sensors are suitable for basic position detection, encoders are suitable for systems requiring higher position feedback accuracy, and sensorless control can reduce the need for position sensor hardware but requires careful evaluation of low-speed and startup performance.

 

For applications such as humanoid robots, quadruped robots, exoskeletons, and robotic arms, selection should also take into account low-speed torque control, continuous current capability, communication interfaces, and overall compatibility between the motor and drive.

 

By evaluating motor specifications, control requirements, and actual operating conditions together, you can select a BLDC motor drive solution that truly meets the needs of your robotic system.

 

FAQ: Frequently Asked Questions

 

1. Why Do Robot Motors Commonly Use FOC Control?

 

Robot joints often need to accelerate and decelerate frequently, rotate in both directions, and dynamically adjust output torque. By controlling the current vector, FOC enables precise torque adjustment and helps improve smoothness during low-speed operation. This makes it a common choice for robotic joint drive systems.

 

2. Does an FOC Drive Always Require an Encoder?

 

No. FOC can use sensored feedback methods such as encoders and Hall sensors, or sensorless rotor position estimation. Encoders provide higher-resolution position feedback and are generally more suitable for applications with demanding low-speed and position control requirements.

 

3. Can Hall Sensors Be Used for FOC Control?

 

Yes. Some FOC drives support Hall sensors as a source of rotor position feedback. However, Hall sensors have relatively low position resolution, so actual control accuracy and low-speed performance also depend on the drive's algorithm design.

 

4. Is Sensorless FOC Suitable for Robot Joints?

 

It depends on the specific application. Conventional back-EMF-based sensorless FOC has difficulty estimating rotor position at zero and extremely low speeds, while robot joints typically require frequent starts and stops, low-speed operation, and stable torque output.

Therefore, before choosing a sensorless solution, its control performance during startup, low-speed operation, and load changes should be thoroughly tested.

 

5. What Is the Difference Between an Encoder and a Hall Sensor?

 

Hall sensors mainly provide rotor magnetic field position information and commutation signals. They have a simple structure and relatively low cost, but limited position resolution. Encoders provide more precise rotor angular position information and are suitable for control systems that require higher position feedback accuracy.

 

6. What Is the Difference Between Sensorless and Sensored Control?

 

Sensored control uses physical devices such as Hall sensors or encoders to obtain rotor position information. Sensorless control estimates rotor position or speed using signals such as voltage, current, and back EMF generated during motor operation. The two methods differ in hardware cost, position feedback accuracy, and low-speed performance.

 

7. Why Is Low-Speed Performance Important for Robot Joints?

 

Robot joints often need to perform precise movements at low speeds and adjust output torque in real time according to load changes. Unstable low-speed operation may cause joint vibration, jerky motion, or reduced control accuracy. Therefore, low-speed performance is an important factor when selecting motor drives for robotics.

 

8. When Choosing a BLDC Motor Driver, Which Is More Important: Peak Current or Continuous Current?

 

Both are important. Peak current determines the drive's short-term output capability, while continuous current determines its long-term operating capability. For robot joints, peak current, continuous current, and peak current duration should all be evaluated based on acceleration, load changes, and the actual motion cycle.

 

9. Do the Motor and Drive Have to Be from the Same Brand?

 

No. Motors and drives from different brands can work together, but their voltage, current, back-EMF parameters, feedback interfaces, control algorithms, and communication protocols must be compatible. For systems requiring high control accuracy, parameter configuration and actual operating tests should also be performed.

Related Articles
2026  Frameless Torque Motors for Robotics Selection Guide
2026 Frameless Torque Motors for Robotics Selection Guide
Explore frameless torque motors for robotics. Compare outrunner and inrunner designs, integration tips, and select the ideal motor for your actuator needs.
Mar 10,2026
Enhancing Human-Robot Collaboration Through Dance Move Learning
Enhancing Human-Robot Collaboration Through Dance Move Learning
Engineers at the University of California San Diego have made significant advancements in humanoid robot technology. They have successfully trained a robot to effortlessly learn and perform a variety of expressive movements, including simple dance routine
Sep 20,2024
RoboTeam Twente Mars Rover Case Study: How CubeMars Meets the Motion Demands of Challenging Terrain
RoboTeam Twente Mars Rover Case Study: How CubeMars Meets the Motion Demands of Challenging Terrain
Discover RoboTeam Twente’s six-wheel Mars rover drive system and explore how the CubeMars AK70-10 KV100 integrated actuator is used for in-wheel drive, along with key considerations for torque, gear ratio, installation space, and multi-motor control in mo
Sep 23,2026
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt