How to choose a suitable underwater thruster
1、Performance parameters
2、Structural characteristics
3、Installation convenience
4、Service life
Advantages of CubeMars DW Series Underwater Thrusters
1、Dive into the deep sea freely
2、Precision-cast alloy, corrosion-resistant and durable
3、Sealing process
4、Shafting design
5、Propeller and fairing

Underwater Thrusters Designed For Depth,Multiple Specification Options

CubeMars / Sep 29,2024

As is widely known, an underwater thruster is a device specifically designed for underwater activities. It can provide power and help divers, submarines, unmanned underwater robots (ROV), and others move rapidly in the underwater environment. Its core component is an efficient electric motor, such as a brushless DC motor. The purpose is to generate thrust through propeller or jet propulsion to push the user or vehicle forward in the water.


As the application fields of underwater thrusters become more and more extensive, including in industries such as ocean exploration, underwater work, resource development, and environmental protection detection, the demand for underwater thrusters will grow greater and the requirements will also become higher, especially in terms of unmanned underwater robots (ROV/AUV). Therefore, choosing a suitable underwater thruster has become a challenge faced by many consumers.


Today, let's briefly discuss 


How to choose a suitable underwater thruster


1、Performance parameters


I. Thrust: Select the appropriate thrust according to the weight of the equipment and its intended use. Generally speaking, the greater the thrust, the stronger the performance of the equipment.


II. Power: The power should match the weight of the equipment and the operating depth. The greater the power, the higher the energy consumption and noise will be.


2、Structural characteristics


Compactness: Choose a model with a compact structure, small size, and light weight, which helps improve operational flexibility.


Self-cleaning function: The blades should have a self-cleaning function to prevent entanglement and blockage by debris and ensure long-term stable operation.


3、Installation convenience


Ease of installation: Ensure that the selected thruster is easy to install and maintain to reduce operating costs and time.


4、Service life


Corrosion resistance: Underwater thrusters are widely used in remotely operated underwater detectors (ROV) and autonomous underwater detectors (AUV). They need to withstand the high pressure and corrosive environment in the deep sea. Therefore, its corrosion-resistant design is crucial.


Service life: Choose those models that have been verified and have good durability. Products with a longer warranty period are usually more reliable.


Underwater Thrusters Designed For Depth,Multiple Specification Options


Underwater Thrusters


The SW and DW series underwater thrusters newly launched by CubeMars adopt a closed design. The key components of the thruster are all placed inside the sealed housing, effectively avoiding damage caused by foreign objects such as sediment and being able to cope with the complex and changeable underwater environment, meeting the application requirements of long life, corrosion resistance, and maintenance-free.


At the same time, the underwater thruster adopts a comprehensive protection design, fully considering the heat dissipation problem generated during operation. The interior is filled with high-efficiency thermal conductive materials, so that the thruster can dissipate heat through immersion in water and achieve efficient operation. The sealed housing of the thruster is strong and durable, with a maximum operating depth of 350 meters, and the maximum mooring thrust covers 7 to 25 kgf, which can meet the surface and underwater application requirements of different levels of ROV, unmanned ship, surfboard, and others.


Advantages of CubeMars DW Series Underwater Thrusters


1、Dive into the deep sea freely


Small size, strong power, with mooring thrust of at least 25 kgf.


DELVE INTO THE DEEP,NAVIGATE WITH EASE


2、Precision-cast alloy, corrosion-resistant and durable


Lightweight and high-strength aluminum alloy, wear-resistant and durable.


ALLOY PRECISION CASTING
CORROSION RESISTANCE
AND DURABILITY


3、Sealing process


Threaded connection process,two-stage independent sealed cabin,and low-resistance dynamic sealing process. 


DESIGNED FOR DEPTH
MULTIPLE SPECIFICATION OPTIONS


4、Shafting design


Simplify the internal structure. In many applications, it is very sturdy and operates stably and reliably.


5、Propeller and fairing


Streamlined design reduces underwater resistance to a greater extent and realizes efficient operation underwater.


INNOVATIVE DESIGN,CUTTING-EDGE ENGINEERING


For more specifications and options of underwater thruster series products, please refer to: SW Series Underwater Thruster and DW Series Underwater Thruster in detail.



Related Articles
How to Choose Hip and Knee Joint Motors for Humanoid Robots
How to Choose Hip and Knee Joint Motors for Humanoid Robots
A comprehensive guide to selecting motors for humanoid robot knee and hip joints, covering torque matching, thermal management, and dynamic response to balance performance and cost across applications.
Mar 25,2026
OpenExo: Modular Open-Source Exoskeleton Powered by CubeMars Robotic Actuators
OpenExo: Modular Open-Source Exoskeleton Powered by CubeMars Robotic Actuators
OpenExo, a modular exoskeleton powered by CubeMars robotic actuators, offering open-source innovation for rehabilitation and human performance enhancement.
Aug 29,2025
Design Challenges and Solutions for Underwater Robot Power Systems
Design Challenges and Solutions for Underwater Robot Power Systems
Explore key challenges in underwater robot power systems, including waterproofing, cooling, efficiency, reliability, and propulsion solutions.
Aug 27,2026
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt