Cubemars - 17 Year Motor Manufacturer info@cubemars.com +86 13755649079
English
English
中文简体
日本語
Deutsch
Français
한국어
Español
Pусский
Quick Registration
Create your CubeMars account

 

Moment

Creat powerful robotic chassis with CubeMars AK series actuator

CubeMars / Apr 13,2022

Nikodem Bartnik created a powerful robotic chassis using CubeMars AK series actuators and Arduino


After attempting to incorporate a few AK80-9 KV100 robotic actuators from CubeMars into a robotic arm project, YouTuber Nikodem Bartnik was forced to pivot to a different kind of project: a universal robotic chassis/platform. By using these high-power and high-precision motors, his robot could be both fast and accurate while moving along the floor.


Once a flat plate had been cut from a piece of plywood with the help of a CNC router, Bartnik mounted the two motors and attached a wheel to each one. To control the motors, he went with a single Arduino Uno and fabricated a custom PCB that routes CAN bus signals between the Uno and the two motors. Power was provided to everything via a pair of LiPo battery packs for a total of around 24 volts. 



Currently, the robot is essentially an RC car that responds to commands that it receives from somewhere else. In Bartnik’s project, he used an additional Uno connected to a laptop over USB and an nRF24 radio transceiver module to wirelessly send data to the robot’s nRF24 module. He also made a Python script, which can be used to set the speed of the robot’s movements and takes arrow key presses that are then converted to directional movements. 


You can watch Bartnik’s video below for more information or you can check out the his repo here for the project code and design files.



Related Articles
CubeMars Empowers the University of Minnesota’s Agricultural Quadruped Robot: Highly Integrated Motors Drive Smart Farming
CubeMars Empowers the University of Minnesota’s Agricultural Quadruped Robot: Highly Integrated Motors Drive Smart Farmi...
The agricultural quadruped robot dog navigates fields, collects data, and performs tasks that traditional wheeled robots and drones cannot handle on complex terrain.
Jun 10,2025
How to Choose Motors for Rehabilitation Robots: Smooth Torque and Low Cogging Matter
How to Choose Motors for Rehabilitation Robots: Smooth Torque and Low Cogging Matter
When selecting motors for rehabilitation robots, smooth torque and low cogging are key. Detailed selection guidelines for hand, exoskeleton, and lower limb stretching devices, plus real-world case studies.
Apr 28,2026
How Many Motors Can A Robot Have
How Many Motors Can A Robot Have
Explains how many motors a robot can have, analyzing engineering factors such as DOF, torque, mechanical design, and system constraints across different robot types.
Nov 03,2023
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt