Moment
TABLE OF CONTENTS
What is a Servo Motor?
Advantages of Servo Motors
How Does a Servo Motor Work?

Servo Motor,How does it work?

CubeMars / Oct 07,2023

What is a Servo Motor?


A servo motor is a type of motor capable of precisely controlling position, speed, and angle. They are typically used in conjunction with feedback systems such as encoders or resolvers to provide real-time position and speed feedback, enabling highly accurate motion control.


Advantages of Servo Motors


Servo motors have numerous advantages, making them widely used in various applications. Here are the main advantages of servo motors:


1. Precision: Servo motors offer highly precise position and speed control. By using feedback systems like encoders or resolvers, they can continuously monitor and adjust positions, resulting in extremely accurate motion.


2. High Performance: Servo motors typically deliver high torque and high-speed output, making them suitable for high-performance motion applications such as robotics, CNC machines, and printing machines.


3. Rapid Response: Servo motors can quickly adjust to meet changing motion requirements. This is crucial for applications that require fast start, stop, or direction changes.


4. Reliability: Servo motors usually have a longer lifespan as they do not use friction-prone carbon brushes or brush rings, reducing maintenance requirements.


5. Flexibility: Servo motors can easily adapt to various motion trajectories and speed requirements, making them highly versatile for a wide range of applications.


6. Precision Repetition: Servo motors can maintain consistent motion and position control across multiple operations, ensuring precise repeatability for products or robot tasks.


7. Adaptability: Servo motors find applications in various fields, including robotics, automation systems, medical devices, aerospace, and more.


8. Feedback System: The use of feedback systems enables closed-loop control, automatically correcting errors and adjusting motor operation for improved stability and reliability.


9. Low Noise: Servo motors typically operate smoothly and generate less noise, suitable for applications that require low-noise operation.


10. Versatility: Servo motors can be used in various mechanical structures and motion requirements, making them widely applicable across different industries.


How Does a Servo Motor Work?


The working principle of a servo motor relies on a feedback loop system that continuously monitors the motor's position or speed and adjusts it for precise control. Here are the basic steps of how a servo motor works:


1. Set Target Position or Speed: The control system initially receives a user or program-defined target position or speed. This target can be a specific position coordinate or a desired angular velocity.


2. Measure Current State: The servo motor is equipped with feedback devices, typically encoders or resolvers, which continuously measure the motor's current position or speed. This information is relayed to the control system.


3. Calculate Error: The control system compares the target position or speed with the current measured position or speed to calculate the error. This error represents the difference between the motor's current position and the target position.


4. Generate Control Signal: The control system uses the error information to generate a control signal, which is then sent to the servo motor. The goal of this control signal is to reduce the error and adjust the motor to the target position or speed.


5. Motor Adjustment: The servo motor adjusts based on the received control signal. If the error is large, the motor will receive a larger control signal to quickly adjust its position or speed. As the error decreases, the control signal diminishes, causing the motor to approach the target more slowly.


6. Feedback Loop: The above process is a continuous loop, repeatedly monitoring the motor's status and making minor adjustments to get closer to or reach the target.


By maintaining continuous feedback and adjustments, Servo Motors achieve highly accurate position or speed control. This precision control makes servo motors suitable for applications that demand high precision and performance, such as robot arms, CNC machines, printing presses, camera gimbals, and more.



Related Articles
Do robots use AC or DC Motors?
Do robots use AC or DC Motors?
Robots can use both AC (alternating current) and DC (direct current) motors, depending on their specific applications and requirements. Each type of motor has its advantages and is chosen based on the particular needs of the robot's tasks.
Oct 16,2023
2026 High Torque Robot Motor Guide: Frameless Motors vs QDD vs Integrated actuators
2026 High Torque Robot Motor Guide: Frameless Motors vs QDD vs Integrated actuators
Compare QDD motors, frameless motors, and integrated actuators for robotics. Learn torque, control, integration, and selection trade-offs.
May 07,2026
What Is a Frameless Torque Motor? Core Advantages in Robot Joint Design
What Is a Frameless Torque Motor? Core Advantages in Robot Joint Design
In-depth analysis of frameless torque motors' core advantages in robot joint design, enabling lightweight, high-torque, and high-precision intelligent robot applications.
May 19,2026
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt