What Is a Quasi Direct Drive (QDD) Motor?
How a QDD Motor Works
1. From High Speed to Usable Torque
2. Preserving Mechanical Feedback
3. Enabling Precise and Dynamic Control
Why Dynamic Robots Demand QDD Architecture
Application-Level Benefits of QDD Motors for Humanoid & Quadruped Robots
Design Considerations When Selecting a QDD Motor
1.Defining Torque and Dynamic Requirements
2.Selecting an Appropriate Reduction Strategy
3.Evaluating Backdrivability and Interaction Needs
4.Verifying Thermal and Continuous Performance
CubeMars QDD Motors for Exoskeletons
Conclusion

2026 Quasi Direct Drive (QDD) Motors for Humanoid & Quadruped Robots Overview

CubeMars / Mar 05,2026

What Is a Quasi Direct Drive (QDD) Motor?


Robotic motors usually fall into two extremes: fully direct drive systems with no gearbox, or high-ratio geared motors that rely heavily on mechanical amplification. Quasi Direct Drive(QDD) motors were introduced as a structural middle ground, redistributing torque generation between the motor and the transmission stage.


The idea of "quasi" is subtle but important. It reflects a deliberate compromise between two design extremes, aiming to preserve responsiveness while keeping the actuator compact and practical.


The Concept of  "Quasi"  Direct Drive


Why not use a pure direct drive motor? Eliminating the gearbox entirely would require the motor to generate all torque electromagnetically, demanding larger size, higher current, and more intensive thermal management.


Conversely, why not rely on a high reduction ratio? Extreme gearing alters the joint's mechanical behavior, making it less responsive and more isolated from external forces.


QDD addresses both limitations by keeping a modest reduction stage while allowing the motor to provide most of the torque. The result is a drivetrain that behaves closer to direct drive, delivering both compactness and mechanical practicality.


ake-90-8-kv35-quasi-direct-drive-motor


How QDD Differs from Traditional Geared Motors


In conventional high-ratio systems, torque is created primarily through mechanical multiplication. A small motor spins at high speed, and the gearbox amplifies torque dramatically before it reaches the joint.


QDD systems invert that relationship.Here, the motor is designed to deliver substantial torque directly. The gearbox no longer dominates output behavior; instead, it fine-tunes torque delivery and supports structural integration.


This shift changes three fundamental characteristics:

  • Reflected inertia at the joint

  • Ease of mechanical feedback (backdrivability)

  • Immediate torque responsiveness


The gearbox becomes a supporting element rather than the defining feature of the motor.


Typical Reduction Ratios in QDD Systems


QDD is not defined by a specific number, but most implementations fall within a 6:1 to 10:1 reduction range.


This range is not arbitrary—it represents an engineering equilibrium.


  • Below it, motor size and electrical demand increase sharply

  • Above it, the system begins to inherit high-ratio limitations, such as slower response and reduced backdrivability


The selected reduction ratio preserves dynamic behavior while keeping motor size and current within practical limits.


How a QDD Motor Works


1. From High Speed to Usable Torque


Every QDD motor begins with a brushless motor. Motors naturally operate at high rotational speeds but generate relatively low torque. If connected directly to a robotic joint, the system would move quickly but struggle under load.


To convert speed into usable torque, QDD systems introduce a low reduction gearbox, typically around 5:1 to 10:1. This means that when the motor rotates multiple times, the joint rotates once. Speed decreases moderately, and torque increases proportionally.


Unlike traditional motors that rely on very high reduction ratios (50:1 or higher), QDD adjusts this balance only slightly. It amplifies torque without heavily isolating the motor from the joint. And this limited reduction is what defines the “quasi-direct” concept.


2. Preserving Mechanical Feedback


Low gear ratios allow bidirectional force transmission:

  • Forward: Motor drives the joint

  • Backward: External forces at the joint travel back through the gearbox and are sensed by the motor


This property — known as backdrivability — is a key differentiator. In high-ratio systems, gears often block reverse force transmission, making joints mechanically stiff. In contrast, QDD maintains mechanical transparency.


Preserved feedback keeps the motor mechanically coupled to the joint, rather than isolating it behind excessive gearing.


3. Enabling Precise and Dynamic Control


With this mechanical transparency, torque control becomes significantly more straightforward. Since the relationship between motor torque and joint torque remains predictable (after simple scaling), the controller can estimate output force accurately using encoder feedback and current sensing.


Instead of only commanding position — "rotate to this angle," the system can command torque directly — "apply this level of force." This capability is critical for robots that must interact with their environment, absorb impacts, or perform dynamic movements.


By combining moderate torque amplification with preserved responsiveness, QDD motors achieve a balance between strength and control — making them especially suitable for legged robots, humanoids, collaborative systems, and wearable robotics.


Key Takeaway:

A QDD motor works by slightly reducing motor speed to increase torque while preserving mechanical feedback, enabling both power output and dynamic responsiveness.


quasi-direct-drive-motor


Why Dynamic Robots Demand QDD Architecture


1. The Shift from Position Control to Force Control

  • Dynamic robots cannot rely solely on position control; high-speed motion requires joints to adapt to external forces.

  • QDD's low gear ratio and mechanical transparency allow motors to directly sense joint torque, enabling precise force-based control.

  • This capability is essential for robots performing agile or unpredictable movements.


2. The Importance of Low Inertia in High-Speed Motion

  • High reduction ratios amplify motor inertia, which slows down joint response and reduces agility.

  • QDD maintains low reflected inertia, keeping joints responsive and enabling fast, precise movements.


3. Energy Efficiency in Mobile Robots

  • High-ratio gearboxes increase friction losses and energy consumption.

  • QDD's compact, low-friction design reduces energy waste, improving battery life and operational efficiency in mobile platforms.


4. Structural Weight Constraints in Multi-DOF Systems

  • Multi-joint robots are sensitive to joint weight; heavy actuators compromise dynamics and efficiency.

  • QDD actuators are lightweight and compact, allowing integration into dense multi-DOF systems without sacrificing performance.

 

Application-Level Benefits of QDD Motors for Humanoid & Quadruped Robots


The architectural characteristics of QDD motors : low gear ratio, low reflected inertia, and torque transparency, are not merely mechanical design choices. They translate directly into performance advantages when implemented in legged robots.


While humanoid and quadruped platforms differ in morphology and locomotion strategy, both rely on rapid force control, dynamic balance, and energy-efficient motion. The table below summarizes how QDD characteristics convert into practical benefits across these two robot categories. The contrast becomes more evident when these two platforms are viewed side by side.


Performance & Benefit Mapping:

QDD CharacteristicHumanoid RobotsQuadruped RobotsSystem-Level Benefit
Low Reflected InertiaFaster balance recovery & stability during single-leg support and external disturbancesRapid leg acceleration & smoother high-speed gait transitionsGreater dynamic stability under real-world disturbances
BackdrivabilityActive compliance for safer human interaction and collaborative environmentsExcellent shock absorption from repeated ground impactsReduced structural stress and improved durability
Precise Torque ControlAccurate coordination of hip–knee–ankle joints in complex movements like stair climbing or squattingReal-time terrain force adaptation across multiple legsHigher control bandwidth and motion smoothness
Low Gear Ratio & Reduced FrictionLower overall power consumption during walking & posture shiftsIncreased locomotion efficiency and reduced actuator heatingExtended operational time and improved energy economy


Why the Benefits Manifest Differently


Although the actuator architecture remains the same, the resulting advantages express themselves differently due to structural and locomotion differences.


In Humanoid Robots


Humanoid stability is fundamentally a balance problem. With a high center of mass and repeated single-leg support phases, even small disturbances can create significant rotational moments around the ankle and hip joints.


In this context, motor responsiveness becomes a stability determinant rather than just a performance parameter.


QDD architecture reduces reflected inertia, enabling rapid corrective acceleration during balance recovery. Rather than resisting disturbances due to drivetrain stiffness, the system remains dynamically adaptive. Backdrivability further enables active compliance — meaning the robot can yield when necessary, rather than fight against unexpected forces.


In practical terms, this translates into:

  • Faster push recovery during walking

  • Smoother weight transfer between legs

  • More natural multi-joint coordination


Rather than moving like a rigid machine, the humanoid behaves with controlled flexibility — a critical characteristic for robots designed to operate near humans.


In Quadruped Robots


Quadruped locomotion is not primarily a balance problem — it is a cyclic impact and propulsion problem.


Each stride involves:


1.  A rapid swing phase

2.  Ground contact with impulsive force

3.  Load transfer across the body

4.  Immediate preparation for the next step


During these high-frequency cycles, motor inertia and friction directly affect gait efficiency and shock tolerance. QDD' low drivetrain impedance enables real-time impact sensing and compensation. At the same time, reduced limb inertia enables quicker leg retraction and repositioning during high-speed motion.


The result is not just smoother movement, but improved locomotion dynamics:

  • More stable high-speed trotting and running

  • Better terrain adaptation under uneven ground conditions

  • Reduced energy loss during repeated impact cycles


For mobile robots operating outdoors, these characteristics directly enhance endurance and terrain robustness.


ake-series-quasi-direct-drive-motor


From Mechanical Design to Performance Advantage


The key strength of QDD architecture lies in its balance: it amplifies torque without isolating the motor from the joint. By avoiding extreme gearing while retaining torque density, the actuator preserves both strength and agility.


  • In humanoid systems, this translates directly into improved stability and safer interaction with the environment.

  • In quadruped systems, it translates into speed, adaptability, and efficiency.


In both cases, QDD does more than improve actuator performance — it enables a higher class of dynamic robotic behavior.

 

Design Considerations When Selecting a QDD Motor


QDD benefits such as responsiveness, transparency, and efficiency become meaningful only when the actuator matches the joint's functional role.

Selection therefore follows a clear sequence: define force demand, shape transmission behavior, and confirm sustainable output.


1.Defining Torque and Dynamic Requirements


Selection starts with what the joint must physically deliver.


Hips and knees require higher continuous torque for support and propulsion. Distal joints prioritize acceleration and low inertia.


Key evaluations include:

  • Peak torque

  • RMS torque over duty cycles

  • Required acceleration bandwidth


Since QDD systems use moderate gear reduction, torque density must come primarily from the motor. Proper sizing balances performance and mass. With torque defined, the next step is determining how it is transmitted.


2.Selecting an Appropriate Reduction Strategy


In QDD architecture, the reduction ratio controls both torque output and mechanical transparency. Lower ratios make joints more responsive and reduce reflected inertia, while slightly higher ratios increase support for sustained loads and reduce motor stress. The right ratio depends on whether a joint prioritizes dynamic motion or continuous load-bearing.


Essentially, the reduction ratio acts as a mechanical lever, translating motor torque into joint behavior. Next, evaluate how the joint should respond to external forces.


3.Evaluating Backdrivability and Interaction Needs


Backdrivability defines how easily a joint reacts to forces from the environment. Joints that encounter impacts or need safe interaction with humans perform better with higher transparency, while joints mainly supporting structure can tolerate stiffer behavior.


The joint's responsiveness to external forces depends on the interplay between motor inertia and gear ratio, which can be adjusted to suit the robot's intended tasks. Once the desired interaction behavior is established, engineers can then verify thermal performance and continuous output to ensure reliable operation over the long term.


4.Verifying Thermal and Continuous Performance


Because QDD relies heavily on motor-generated torque, thermal capacity is critical.


Engineers should prioritize:

  • Continuous torque ratings

  • RMS current under real duty cycles

  • Cooling limits within the mechanical envelope


Thermal alignment ensures dynamic performance can be sustained without degradation.


Transition to Implementation


When these considerations are addressed together, QDD motors can be precisely tailored to the functional demands of humanoid and quadruped robotic joints, enabling dynamic performance that aligns with system-level requirements.

 

CubeMars QDD Motors for Exoskeletons


When designing hip and knee joints for dynamic humanoids, engineers face a clear challenge: delivering high continuous torque while preserving fast corrective response.


For high-speed quadruped locomotion, the priority shifts toward rapid leg swing, impact tolerance, and efficient cyclic force control.


The CubeMars AKE series was developed precisely for these real-world joint demands.


QDD Architecture in the AKE Series


Rather than merely adopting low-ratio gearing, the AKE series integrates QDD principles at the structural level:

  • Low Reduction Ratio – minimizes reflected inertia, keeping joint response fast and smooth

  • High Torque Density – delivers substantial torque in a compact form factor, optimizing motor efficiency

  • Force Feedback Capability – maintains mechanical transparency for precise torque control and dynamic interaction


These design choices ensure that the AKE actuators not only retain the key benefits of QDD but also remain practical for integration, thermal management, and structural constraints.


applications-of-ake-series-quasi-direct-drive-motor


Matching Motor Size to Joint Function


In a humanoid robot:

  • Hip and knee joints must handle continuous load-bearing and propulsion

  • Distal joints prioritize responsiveness and low inertia


In a quadruped platform:

  • Proximal joints stabilize body mass

  • Distal joints execute high-frequency swing cycles


The AKE series provides scalable actuator sizes to align with these functional roles:

ModelQDD-Relevant ParameterTypical ApplicationPerformance FocusKey Benefit
AKE90-8 KV35

Max Continuous Torque: 90 Nm / 

Reflected Inertia: 0.08 kg·m² / 

Gear Ratio: 8:1

Hip / KneeHigh continuous torqueSupports stable walking, push recovery, and heavy load-bearing
AKE80-8 KV30

Max Continuous Torque: 40 Nm / 

Reflected Inertia: 0.04 kg·m² /

Gear Ratio: 8:1

Mid-size jointsBalanced torque & responsivenessSmooth multi-joint coordination for complex motion
AKE60-8 KV80

Max Continuous Torque: 15 Nm /

Reflected Inertia: 0.015 kg·m² / 

Gear Ratio: 8:1

Lightweight distal jointsLow inertia & high responsivenessHigh-speed adaptation, impact absorption

 

Instead of adapting one motor across all joints, engineers can distribute performance characteristics according to mechanical role.


Designed for Humanoid and Quadruped Platforms


Beyond single-joint performance, the AKE series supports full system integration:

  • Dynamic Control Ready – low reflected inertia and high transparency improve balance and fluid motion

  • Torque Control Compatible – precise force control supports safe human-robot interaction and environmental responsiveness

  • Modular Integration – multiple motor models can be combined to cover entire robot kinematics, seamlessly adapting to both Humanoid and Quadruped designs


From QDD Advantage to Practical Implementation


The QDD characteristics discussed earlier—low reflected inertia, responsiveness, and torque transparency—are fully realized in the AKE series:

  • Humanoid Robots: enhanced single-leg support stability, improved multi-joint coordination, and safer physical interactions

  • Quadruped Robots: high-speed gait stability, better terrain adaptability, and lower energy consumption


By translating theoretical QDD advantages into tangible actuator design, the AKE series enables robots to achieve a higher level of dynamic performance in both legged platforms.


Conclusion


Quasi Direct Drive (QDD) motors represent a structurally balanced approach to robotic joint design. By integrating moderate gear reduction with high torque density, they preserve mechanical transparency while maintaining precise control accuracy. Rather than pursuing extreme reduction ratios or eliminating gearing altogether, QDD architecture establishes a more measured distribution of torque generation and transmission within the joint.


For humanoid and quadruped robots operating in dynamic environments, this structural balance translates into improved responsiveness, stable force interaction, and reliable motion control. In summary, Quasi Direct Drive (QDD) motor is not merely a component-level decision; it serves as a foundational factor that directly influences overall robotic performance.


Related Articles
CubeMars Announces Sponsorship for the 2024 ROBOCON University Robot Contest to Boost the Global Robotics Market
CubeMars Announces Sponsorship for the 2024 ROBOCON University Robot Contest to Boost the Global Robotics Market
ROBOCON, as a significant event in the field of robotics worldwide, has continuously nurtured technical talents for the global robotics industry. In a bid to further propel the development of robotics technology globally and foster the next generation of
Oct 20,2023
Innerunning gimbal motor G60
Innerunning gimbal motor G60
The Innerunning gimbal motor G60 adopts a large hollow shaft design, which can be integrated with an electric slip ring for easy to cross the cables.
Aug 22,2023
Complex Environment Robot Motor Applications: From Space Exploration and Extraterrestrial Missions to Long-Term Unmanned Operation
Complex Environment Robot Motor Applications: From Space Exploration and Extraterrestrial Missions to Long-Term Unmanned...
Motor selection for robots operating in complex environments should not focus solely on individual parameters such as peak torque and speed. Instead, it requires a comprehensive evaluation based on the actual operating conditions, robotic tasks, mechanica
Sep 28,2026
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt