Addressing the Challenge of High-Cost Prosthetics
The Role of CubeMars Motors

Nepali Student Team Develops Low-Cost Ankle-Foot Prosthesis Prototype Using CubeMars AK60-6 Motor

CubeMars / Mar 25,2025

Recently, a team of Nepali students successfully developed an ankle-foot prosthesis prototype based on the CubeMars AK60-6 V1.1 robotic actuator and subjected it to rigorous testing. The project aims to provide affordable and high-performance prosthetic solutions for developing countries like Nepal.


high-performance prosthetic solutions


Addressing the Challenge of High-Cost Prosthetics


Ankle-foot prostheses are essential assistive devices that help lower-limb amputees regain mobility. However, traditional prosthetics are often expensive and inaccessible in developing countries. To tackle this challenge, the student team developed a cost-effective ankle-foot prosthesis prototype based on hip motion tracking.


a cost-effective ankle-foot prosthesis prototype


Utilizing 3D printing technology, the team manufactured the prosthesis shell and structural components, significantly reducing production costs while maintaining strength. This design, combined with the high performance of the AK60-6 motor, makes the prosthesis an ideal solution for patients in developing countries.



The Role of CubeMars Motors


The CubeMars AK60-6 V1.1 robotic actuator motor played a crucial role in the project:


  • High Torque and Precise Control: The AK60-6 V1.1 robotic actuator delivers the necessary high torque output for prosthetic movement while ensuring precise position control, allowing the prosthesis to accurately simulate a natural gait.

  • Fast Response: In dynamic motion tests, the AK60-6 motor demonstrated exceptional responsiveness, quickly adapting to the user’s movement changes.

  • Reliability and Durability: Through rigorous load and backdrive testing, the AK60-6 motor proved its reliability and durability over long-term use, meeting the high standards required for medical devices.


The prosthesis prototype has now passed initial testing, and the team plans to conduct further clinical validation to ensure its safety and effectiveness in real-world applications. Moving forward, CubeMars will continue to support such innovative projects, driving the development of affordable, high-performance medical technology to benefit patients worldwide.




Related Articles
How Robotic Actuators Enable More Flexible Motion Applications in Robots
How Robotic Actuators Enable More Flexible Motion Applications in Robots
Explore how robotic actuators improve robot motion performance, from humanoid robots to real-world applications, with CubeMars AK Series solutions.
Jul 29,2026
Boston Dynamics,Shift from Hydraulic to Electric Actuation: A New Era in Robotics
Boston Dynamics,Shift from Hydraulic to Electric Actuation: A New Era in Robotics
Recently, Boston Dynamics announced the retirement of its hydraulically actuated bipedal humanoid robot, Atlas. However, less than 24 hours later, they unveiled the fully electric Atlas robot. As a pioneer and leader in the global robotics industry, Bosto
May 23,2024
Enhancing Human-Robot Collaboration Through Dance Move Learning
Enhancing Human-Robot Collaboration Through Dance Move Learning
Engineers at the University of California San Diego have made significant advancements in humanoid robot technology. They have successfully trained a robot to effortlessly learn and perform a variety of expressive movements, including simple dance routine
Sep 20,2024
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt