Why Does QDD Actuator Selection Require Comprehensive Evaluation?
Key Performance Indicators to Consider When Selecting a QDD Actuator
How to Choose the Right QDD Actuator for Different Robotic Applications?
QDD Actuator Selection Process: From Requirement Definition to Final Model Selection
Recommended CubeMars AKE Series QDD Actuators
Conclusion

How to Choose QDD Actuators? Key Metrics and Application Considerations

CubeMars / Jun 16,2026

With the rapid development of robotics technology, emerging applications such as humanoid robots, quadruped robots, and exoskeletons are continuously driving the advancement of actuator technology. Compared with traditional industrial equipment, modern robots place higher demands on joint systems: actuators must not only provide sufficient power output, but also deliver fast response, precise control, and excellent interaction capabilities.


During robotic motion, joint actuators directly affect the overall movement performance of the robot. Whether it is a humanoid robot performing walking and dynamic balancing, or an exoskeleton device assisting human movement, actuators must achieve efficient power output within a limited space while maintaining flexible and safe motion characteristics.


Traditional servo actuators typically rely on transmission structures with high reduction ratios to increase output torque. However, in some robotic applications that require high dynamic response and force interaction capabilities, excessive mechanical stiffness may limit the backdrivability and motion flexibility of the actuator.


Against this background, QDD (Quasi Direct Drive) actuators have gradually become an important solution for robotic joint design. By adopting a low reduction ratio transmission structure, QDD actuators can achieve a better balance between output capability, response speed, and mechanical compliance, enabling robotic joints to achieve more natural movement patterns.


However, as QDD actuators continue to expand into more application fields, different robotic platforms have also developed significantly different requirements for actuator performance. An actuator suitable for a robotic arm may not necessarily meet the dynamic performance requirements of legged robot joints. Therefore, when selecting a QDD actuator, developers cannot focus on a single parameter alone, but need to evaluate whether the actuator meets the actual application requirements from an overall performance perspective.


Why Does QDD Actuator Selection Require Comprehensive Evaluation?


why-does-qdd-actuator-selection-require-comprehensive-evaluation


A QDD actuator is not simply a combination of a motor and a reduction mechanism, but a core power unit within a robotic motion system. It needs to simultaneously handle multiple tasks, including power transmission, motion control, and interaction with the external environment.


In practical robot design, actuator performance directly affects:


  • Motion speed and agility

  • Posture stability

  • Energy efficiency

  • Human-robot interaction safety

  • Long-term operational reliability


For example, in humanoid robots, leg joints frequently experience acceleration, deceleration, and impact loads. Actuators must not only provide instantaneous high torque but also have the ability to rapidly adjust joint states. In exoskeleton robots, actuators place greater emphasis on lightweight design and backdrivability to ensure that the device can follow human movements and provide natural assistance.


Therefore, when selecting a QDD actuator, developers need to consider the specific application scenario and make a comprehensive evaluation based on multiple key performance factors, including output capability, dynamic response, control accuracy, and mechanical design.


Only by achieving the right balance among these factors can an actuator truly meet the motion requirements of a robotic system. The following sections will analyze the key performance indicators that should be considered during QDD actuator selection, helping developers better understand how different parameters influence practical applications.


Key Performance Indicators to Consider When Selecting a QDD Actuator


key-performance-indicators-to-consider-when-selecting-a-qdd-actuator


The core advantage of QDD actuators lies in their low reduction ratio transmission design, which allows motor output to be transferred more directly to robotic joints, improving system response speed and motion flexibility.


However, for robotic applications, actuator performance is not determined by a single parameter. Different performance indicators often interact with each other. For example, higher output torque usually requires a larger mechanical structure, while a more lightweight design may place higher demands on thermal management and long-term reliability.


Therefore, when selecting a QDD actuator, developers need to evaluate the actuator from multiple perspectives, including power output, motion control, and mechanical performance, based on the overall requirements of the robot system.


In general, the following key performance indicators determine whether a QDD actuator can meet the actual requirements of a robotic platform.

 

Torque Density: Measuring Power Efficiency Within a Limited Space


The requirements for robotic joints are not simply about achieving higher output torque. Under limitations in installation space and overall weight, achieving more efficient power output has become a key direction in modern robotic actuator design.


Torque density is commonly used to measure how much output capability an actuator can provide within a limited weight and volume.


For joints installed at the end of a mechanical structure, actuator weight directly affects the overall inertia performance of the robot. Improving torque density can help robots achieve:


  • Lighter joint structures

  • Lower motion inertia

  • Higher motion efficiency


This is especially important for humanoid robots, quadruped robots, and exoskeleton systems, where joints frequently need to perform rapid start-up, acceleration and deceleration, posture adjustment, and dynamic balance control. These movements require actuators with stronger power response capabilities.


In QDD structures, due to the adoption of a lower reduction ratio design, the motor takes on more of the output task. Therefore, motor performance, magnetic circuit design, and overall structural optimization all influence the final torque density.

 

Peak Torque and Continuous Torque: Do Not Focus Only on Maximum Output


During robotic operation, actuators are not always under the same load conditions.


Different motion phases require significantly different torque capabilities:


Operating ConditionActuator Requirement
Jumping and rapid turningHigh peak output for a short period
Normal walkingStable continuous output
Posture maintenancePrecise torque control


Therefore, when selecting a QDD actuator, developers should consider:


  • Peak Torque

  • Rated Torque

  • Continuous operation capability

  • Thermal management performance


Peak torque determines the actuator's ability to handle short-term high-load situations, while continuous torque determines long-term operational stability. Focusing only on peak torque specifications may overlook temperature rise issues during real-world operation.


For platforms involving frequent dynamic movements, peak output capability and response performance should be prioritized. For systems requiring long-term operation, continuous load capacity and thermal design become more important.

 

Backdrivability: A Key Advantage of QDD Over Traditional Actuators


Traditional high-reduction-ratio actuators usually emphasize output stiffness and mechanical power amplification capability.


However, as robots enter dynamic interaction scenarios, actuators also need to detect external forces and adjust their output states accordingly.



Traditional ActuatorQDD Actuator
Mechanical impedanceHigherLower
Response to external forcesRelatively limitedMore natural
Force interaction controlMore challengingBetter suited


Backdrivability means that robotic joints can respond more naturally to external forces, providing:


  • Improved human-robot interaction safety

  • Better force control performance

  • Enhanced compliant motion capability


For example, exoskeleton robots need to follow human movements, while collaborative robots need to quickly adjust their output when interacting with the environment. The low reduction ratio design of QDD actuators reduces mechanical transmission resistance, allowing the system to achieve lower mechanical impedance.


However, it is important to note that better backdrivability does not mean lower stiffness is always better. A well-designed actuator needs to achieve a balance between output capability, control stability, and mechanical compliance.


Backlash and Control Accuracy: Affecting Final Motion Performance


The final motion accuracy demonstrated by a robot does not depend solely on the control algorithm. The precision of the mechanical transmission system also determines whether joint movements can be accurately executed.


Clearance between gears in a reduction mechanism can cause backlash.


Its impact process can generally be described as:


Mechanical clearance increases → Position errors accumulate → Feedback correction increases → Motion stability decreases


Therefore, for high-precision applications such as robotic arms and dexterous manipulation robots, developers should pay close attention to:


  • Reduction mechanism design

  • Encoder resolution

  • Feedback response speed

  • Control algorithm compatibility


A low-backlash design helps actuators achieve more precise joint control.

 

Dynamic Response: Determining Whether Robot Motion Feels Natural


Modern robots are evolving from simple repetitive movements toward more complex dynamic motions. During this transition, actuators need to continuously perform:


State detection → Control calculation → Output adjustment


For example:


  • Humanoid robots maintaining balance

  • Quadruped robots adapting to terrain changes

  • Robots rapidly adjusting their posture


Dynamic response capability is mainly influenced by:


  • Motor inertia

  • Transmission structure

  • Control system response speed

  • Feedback system performance


A faster response speed helps robots reduce motion delays and quickly recover their state when affected by external disturbances.

 

In summary, QDD actuator selection requires comprehensive evaluation across multiple performance dimensions. Different robotic applications place different priorities on these indicators. Only by matching actuator characteristics with actual requirements can the advantages of QDD technology be fully realized.


How to Choose the Right QDD Actuator for Different Robotic Applications?


how-to-choose-the-right-qdd-actuator-for-different-robotic-applications


Although QDD actuators offer high response speed, low mechanical impedance, and excellent force control capabilities, different robotic platforms do not always prioritize the same actuator characteristics.


In practical development processes, actuators are not simply about choosing the model with the highest specifications. Instead, the selection should be based on:


  • Joint position

  • Motion patterns

  • Load characteristics

  • Control requirements


to find the most suitable actuator solution.


For example, legged robots need to handle frequent impacts and dynamic movements, while robotic arms place greater emphasis on motion accuracy and stable output.


Therefore, the key to QDD actuator selection is not finding the product with the “highest performance,” but achieving the best match between the robot's requirements and the actuator's capabilities.

 

Humanoid Robots: Balancing Power Output and Dynamic Response


Humanoid robots aim to replicate human-like movement patterns, meaning their joint motions have strong dynamic characteristics.


During walking, climbing stairs, and maintaining balance, key joints such as the hip, knee, and ankle need to continuously adjust output torque, allowing the robot to adapt to constantly changing postures.


This means actuators must not only provide sufficient power output but also respond quickly to control system commands.


Humanoid robots typically focus on:


Key RequirementActuator Requirement
Complex dynamic movementsFast response capability
Limited joint spaceHigh torque density
Posture adjustmentStrong force control performance
Long-duration motionLightweight design


Higher torque density can reduce the load on robotic joints, while faster response capability helps the system achieve more natural and stable motion performance.

Especially for critical leg joints, actuators need to balance both output capability and dynamic control performance.

 

Quadruped Robots: Handling Impacts and Rapid Posture Adjustment


Compared with humanoid robots, quadruped robots experience more significant external impacts during movement.


During running, jumping, and traversing complex terrain, leg joints frequently experience:


  • Ground impacts

  • Instantaneous load changes

  • Rapid posture adjustments


Therefore, quadruped robots place greater emphasis on actuator power performance and reliability.


During actuator selection, key factors usually include:


  • Peak torque

  • Continuous output capability

  • Response speed

  • Mechanical reliability


If the actuator output is insufficient, the robot may experience unstable gaits, reduced motion efficiency, and other performance issues.


A QDD actuator with strong dynamic performance can help robots quickly adjust joint states and improve motion adaptability in complex environments.

 

Exoskeletons: Beyond Power Output, Natural Interaction Matters More


The biggest difference between exoskeletons and other robotic applications is that exoskeleton actuators directly participate in human movement. Therefore, they must not only provide assistive power but also avoid restricting natural human motion.


Compared with simply pursuing higher output capability, exoskeleton systems place greater emphasis on:


  • Actuator weight

  • Backdrivability

  • Motion compliance

  • Control accuracy


Good backdrivability reduces joint mechanical impedance, allowing the device to follow human movements more naturally.


At the same time, lightweight design reduces the burden on users and improves comfort during long-term use. For rehabilitation robots and assistive devices, the coordination between the actuator and the human body is often more important than pure peak performance.

 

Robotic Arms and Collaborative Robots: Accuracy and Stability Come First


Robotic arms and collaborative robots typically perform precision operation tasks, so their actuator requirements differ from those of legged robots.


These applications may not require extremely high instantaneous output, but place greater importance on:


  • Joint positioning accuracy

  • Smooth motion performance

  • Torque control capability

  • Long-term operational stability


Especially in tasks such as grasping, assembly, and human-robot collaboration, robots need to precisely control every joint movement.


Focus AreaInfluencing Factors
Motion accuracyBacklash control, encoder feedback
Control stabilityControl algorithms, response speed
Long-term operationThermal management and reliability


Low-backlash structures and high-precision feedback systems help robotic arms achieve more accurate motion control and improve repeatability during complex tasks.

 

Matching QDD Actuator Performance with Application Requirements


Different robotic applications demonstrate that there is no single standard for QDD actuator selection.


Different scenarios prioritize different performance characteristics:


Application TypeKey Performance Focus
Humanoid robotsTorque density, dynamic response, lightweight design
Quadruped robotsPeak torque, impact resistance, reliability
ExoskeletonsWeight, backdrivability, compliance
Robotic armsAccuracy, backlash, control performance


Therefore, when designing robotic joint systems, developers need to select actuators based on actual motion requirements rather than simply comparing a single parameter.


Only after clearly defining application needs and selecting a QDD actuator with matching performance characteristics can the advantages of quasi-direct drive technology be fully realized.


QDD Actuator Selection Process: From Requirement Definition to Final Model Selection


During the development of robotic systems, actuator selection usually involves multiple stages. Developers need to first determine the actual operating conditions of the robot joint, and then gradually filter actuators that meet the required performance, mechanical, and control requirements.


A complete actuator selection process typically includes the following steps:

 

Step 1: Define the Target Joint Instead of Looking at Actuator Specifications First


A QDD actuator is not an independent power component. Its performance needs to match the requirements of the robotic joint where it is installed.


Therefore, during the early stage of selection, developers should first determine:


  • Actuator installation position

  • Joint motion direction

  • Motion frequency

  • Operating mode


For example, even within the same robotic leg, the hip, knee, and ankle joints experience different loads and therefore have different actuator requirements.

Only after the joint’s specific tasks are defined can developers determine what level of actuator performance is actually needed.

 

Step 2: Estimate the Actual Load Based on Motion Conditions


After determining the joint application, the next step is to analyze the forces and loads experienced by the actuator during operation.


The load in robotic motion is usually not constant, but changes with different movement phases:


  • Static state → Support load

  • Acceleration phase → Inertial load

  • Collision or jumping → Instantaneous impact load


Therefore, developers need to evaluate the following based on the motion trajectory:


  • Required peak torque

  • Continuous output requirements

  • Operating duration

  • Thermal conditions


This step determines the required power level of the actuator.

 

Step 3: Select Models That Meet the Performance Requirements


After completing load analysis, developers can move on to selecting specific actuator models.


At this stage, different actuators should be compared based on:


  • Torque density

  • Speed range

  • Backdrivability

  • Control accuracy

  • Response speed


It is important to note that trade-offs often exist between different performance characteristics.


For example:


  • Higher output capability may result in larger size and weight

  • Lower mechanical impedance may require sacrificing some transmission stiffness


The final selection should focus on the overall objectives of the robotic system rather than maximizing a single parameter.

 

Step 4: Confirm Whether the Actuator Can Be Integrated into the System


Even after the actuator meets the performance requirements, it is still necessary to verify whether it can be practically integrated into the robot system.


Common engineering challenges include:


  • Insufficient installation space

  • Incompatible mounting interfaces

  • Difficult cable routing

  • Limited heat dissipation conditions


This is especially important for robots with many degrees of freedom, where the size and weight of each actuator can directly influence the performance of the entire system.

 

Step 5: Validate Long-Term Performance Under Real Operating Conditions


After the initial actuator selection, further testing is required to verify whether the actuator meets actual application requirements.


Key evaluation factors include:


  • Temperature rise during long-term operation

  • Stability during repeated movements

  • Performance under extreme loads

  • Consistency of control response


Because laboratory specifications cannot fully represent the real operating performance of a robot.


Only through validation under actual working conditions can developers determine whether an actuator is truly suitable for the target application.


Recommended CubeMars AKE Series QDD Actuators


recommended-cubemars-ake-series-qdd-actuators


For robotic developers, selecting a QDD actuator requires more than focusing on individual performance parameters. It is also necessary to evaluate whether the actuator can meet the actual requirements of specific joint applications.


An excellent QDD actuator needs to achieve a balance between output capability, dynamic response, control accuracy, and system integration. Based on the demand for high-performance power systems in robotic joints, the CubeMars AKE Series Quasi Direct Drive Actuator adopts a highly integrated design that optimizes the combination of the motor, reduction mechanism, and drive system, providing a compact, efficient, and reliable power solution for robotic joints.


The AKE Series covers different sizes and output levels, meeting the requirements of various applications ranging from lightweight robotic joints to high-load motion platforms.

 

High Torque Density Design for Improved Robotic Motion Efficiency


In robotic systems, actuator weight directly affects the overall motion performance.


This is especially important for dynamic platforms such as humanoid robots and quadruped robots, where joints frequently perform acceleration, deceleration, and posture adjustments. Excessive actuator weight increases motion inertia, requiring the robot to consume more energy to complete movements.


Therefore, high torque density has become a key factor in QDD actuator selection.


The CubeMars AKE Series optimizes motor structures and transmission solutions to provide high output capability while maintaining a compact form factor, enabling better adaptation to the space limitations of robotic joints.


Different AKE models are designed for different load requirements:


Product ModelPeak TorqueKey FeaturesRecommended Applications
CubeMars AKE60-8 KV8012.5 NmCompact and lightweight, high response, suitable for space-limited applicationsSmall robots, dexterous joints, lightweight mechanical structures
CubeMars AKE80-8 KV3030 NmHigher output capability while balancing size and power performanceHumanoid robot and quadruped robot joints
CubeMars AKE90-8 KV3045 NmHigher torque output for high-load applicationsHigh-load robotic joints, complex motion platforms



Through different specifications and model combinations, the AKE Series enables developers to select a more suitable power solution based on the structural requirements of their robots.

 

High Response and Low Mechanical Impedance for Dynamic Robot Applications


Modern robots are evolving from simple repetitive movements toward dynamic and interactive motion.


When humanoid robots maintain balance, quadruped robots adapt to complex terrain, or collaborative robots perform force-controlled operations, actuators need to quickly sense and respond to changes in joint states.


The QDD structure reduces the reduction ratio, allowing motor output to be transferred more directly to the joint, thereby lowering mechanical impedance and improving dynamic response capability.


The CubeMars AKE Series adopts a quasi-direct-drive design, enabling the actuator to achieve:


  • Fast torque response

  • More natural backdrivable motion

  • More flexible joint control


This makes the AKE Series especially suitable for robotic applications requiring high dynamic performance, such as legged robots, exoskeleton systems, and high-degree-of-freedom robotic platforms.

 

Integrated Design for Simplified Robotic Joint Development


Robotic actuators need to satisfy performance requirements while also reducing system development complexity.


Traditional robotic joints often require separate components such as:

  • Motors

  • Gear reducers

  • Drivers

  • Encoders

  • Mechanical connection structures


Multiple independent modules increase mechanical design complexity and raise system integration and debugging costs.


The CubeMars AKE Series adopts an integrated joint actuator design, combining core components into a compact structure, allowing developers to build robotic joints more efficiently.


Its integration advantages include:


Design FeatureBenefits
Integrated motor and reduction mechanismReduces mechanical design complexity
Integrated drive systemSimplifies control system deployment
Compact structural designImproves robot space utilization
Modular interfacesEnables faster integration and testing


For robotic projects requiring rapid development and iteration, integrated QDD actuators can effectively lower the development barrier.

 

AKE Selection Recommendations for Different Robotic Platforms


Different robotic applications emphasize different actuator characteristics. Therefore, actuator selection should be matched according to actual motion requirements.


Application ScenarioRecommended AKE Model DirectionKey Performance Focus
Lightweight robotic jointsCubeMars AKE60-8 KV80Weight, response speed, space utilization
Humanoid robot leg jointsCubeMars AKE80-8 KV30Torque density, dynamic output, reliability
High-load motion platformsCubeMars AKE90-8 KV30Output capability, continuous operation performance


By selecting suitable models for different joint positions, the AKE Series helps robotic systems achieve a balance between power performance, control accuracy, and mechanical design.


The CubeMars AKE Series QDD actuators are characterized by high integration, fast response capability, and a wide range of specifications, providing robotic developers with more flexible joint drive solutions.


Conclusion


With the continuous development of humanoid robots, quadruped robots, and intelligent robotic systems, actuators have evolved from simple power output components into core elements that influence robotic motion performance, control capability, and interaction experience.


Compared with traditional drive solutions, QDD actuators provide a better balance between power output, dynamic response, and backdrivability through their low reduction ratio design, creating new possibilities for modern robotic joint development.


During the QDD actuator selection process, developers should not focus on a single parameter alone. Instead, they need to comprehensively evaluate factors such as torque density, continuous output capability, backdrivability, control accuracy, and system integration capability based on actual application requirements.


Different robotic platforms have different actuator demands. Only by selecting actuators that match the mechanical design and motion tasks can the full performance potential of the robotic system be achieved.


The CubeMars AKE Series is optimized around robotic joint application requirements. Through a highly integrated design, compact structure, and multiple product options, it provides flexible and reliable power solutions for various types of robots.


Whether for lightweight robotic joints or complex motion platforms requiring high dynamic response, selecting the right QDD actuator solution allows robotic developers to achieve a better balance between power output, control accuracy, and motion flexibility.

Related Articles
MenteeBot: The Shopping Robot with Exceptional Abilities
MenteeBot: The Shopping Robot with Exceptional Abilities
imagine walking into a shopping mall, and a 1.7-meter tall, 70-kilogram "robot clerk" warmly greets you: "How can I assist you today?"
Aug 28,2024
RO Lite: Engineered for Lightweight Performance
RO Lite: Engineered for Lightweight Performance
Get ready for the CubeMars RO Series frameless motor lightweight edition
Feb 26,2024
Eelume:Revolutionizing Underwater Intervention
Eelume:Revolutionizing Underwater Intervention
Until now, underwater inspection and maintenance have heavily relied on underwater vehicles supported by surface vessels. However, Eelume, a new type of underwater intervention tool, is set to change everything.
Jul 31,2024
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt