- Why Do Mars Rovers Need Special Drive Motors?
- Key Specifications for Mars Rover Motor Selection
- Why Do Mars Rover Projects Choose CubeMars Motors?
- CubeMars Powers the RoboTeam Twente Mars Rover
- AK45-36 KV80: Providing a High Reduction Ratio and Strong Output Capability
- AK70-10 KV100: Balancing Power Output and Dynamic Response
- Why Does RoboTeam Twente Choose CubeMars Motors?
- What Types of Robots Are CubeMars Drive Solutions Suitable For?
- How to Choose the Right Motor for Your Mars Rover?
- Conclusion
Mars Rover Motor Selection Case: How Does CubeMars Drive Solution Handle Challenging Terrain?
Mars Rovers are a type of mobile robot that places extremely high demands on the drive system.
Compared with ordinary wheeled robots, Mars Rovers need to operate in more complex environments, such as:
Soft sandy terrain
Gravel roads
Irregular obstacles
Long-distance travel
High-slope terrain
These environments place higher demands on the drive system.
An excellent Mars Rover drive solution not only needs to provide sufficient output torque, but also needs to take into account:
High torque density
Compact structure
Precise motion control
High reliability
Long-term stable operation capability
Therefore, during the motor selection process for a Mars Rover, engineering teams typically do not focus on a single parameter, such as maximum torque or maximum speed, but need to comprehensively evaluate whether the entire drive system can meet the motion requirements in complex environments.
In recent years, more and more robotics projects have begun adopting highly integrated robotic actuators , among which CubeMars motor solutions have already been applied to Mars Rovers, mobile robots, and other robotic platforms, providing power support for complex motion systems.
Why Do Mars Rovers Need Special Drive Motors?
Mars Rovers typically adopt multi-wheel drive structures, such as four-wheel, six-wheel, or even more wheel configurations.
During actual operation, the vehicle needs to deal with:
Changes in ground resistance
Increased climbing load
Impact from obstacles
Risk of wheel slippage
Space and weight limitations
Therefore, Mars Rover drive motors cannot simply pursue high-speed performance, but need to focus on the following aspects.
1. High Output Torque: Ensuring Traversability on Complex Terrain
Mars Rovers need to rely on their wheels to generate sufficient driving force to overcome:
Their own weight
Ground friction
Slope resistance
Obstacle resistance
Wheel-end output torque is usually affected by the following factors:
Output Torque = Motor Torque × Reduction Ratio × Transmission Efficiency
Therefore, increasing output torque within a limited space is an important direction in robotic drive system design.
2. High Torque Density: Achieving Greater Power Within a Limited Weight
For Mars Rovers, weight directly affects:
Energy consumption
Operating time
Structural load
Off-road capability
Compared with simply increasing motor size, a high torque density design can provide greater output capability with a smaller volume and lower weight.
This is also an important reason why highly integrated drive modules are receiving increasing attention in the robotics field.
3. Precise Control: Enabling Coordinated Multi-Wheel Motion
Mars Rovers usually have multiple drive wheels.
To ensure stable vehicle motion, the motors need to provide:
Position feedback
Speed control
Torque control
Closed-loop motion control capability
Precise feedback can help the control system:
Adjust wheel speed
Reduce slippage
Improve obstacle-crossing capability
Improve motion stability
4. High Reliability: Meeting Long-Term Operation Requirements
Mars Rovers, lunar rovers, and outdoor mobile robots typically need to operate for long periods of time.
Therefore, the drive system needs to provide:
Stable mechanical structure
Good heat dissipation capability
Reliable control performance
Continuous load capability
Key Specifications for Mars Rover Motor Selection
1. Motor Torque
Torque determines how much driving force the robot can generate.
For mobile robots, peak torque can help the system handle:
Climbing slopes
Sudden loads
Passing obstacles
However, actual motor selection cannot focus only on peak torque; continuous output capability also needs to be considered.
2. Reduction Ratio
The reduction mechanism determines the speed and torque at the motor output.
A higher reduction ratio can generally provide:
Greater output torque
Better low-speed driving capability
While a lower reduction ratio can provide:
Faster response
Higher motion speed
Therefore, matching needs to be carried out according to the vehicle weight, wheel diameter, and target speed.
3. Motor Size and Weight
Mars Rovers are usually highly sensitive to space and weight.
Traditional drive systems may require:
Motor
Gearbox
Encoder
Driver
Multiple components are installed separately.
This solution increases:
Structural complexity
Assembly difficulty
System weight
Therefore, highly integrated robotic actuators have become the choice for an increasing number of projects.
Why Do Mars Rover Projects Choose CubeMars Motors?
1. High Torque Density: Strong Driving Force in a Small Size
Traditional solutions usually require:
Motor + External Gearbox + Encoder + Driver
This structure can result in:
Increased volume
More complex installation
Increased system weight
In contrast, the CubeMars AK Series adopts an integrated design that integrates multiple core components, making robot designs more compact.
For Mars Rovers, this means:
Smaller installation space
Lower overall vehicle weight
Higher power output efficiency
This is also an important reason why robotics teams choose CubeMars as their drive solution.
2. Planetary Gear Reduction Structure: Balancing Torque and Reliability
Mars Rovers need to operate at low speeds and under high loads.
The planetary reduction structure offers advantages such as:
High load-bearing capacity
High transmission efficiency
Compact size
Relatively high reduction ratio
and other advantages.
CubeMars AK Series adopts an integrated planetary reduction structure, which can help mobile robots achieve higher wheel-end output torque.
For example:
AK70-10 KV100 adopts a 10:1 planetary reduction structure, which improves output capability while maintaining dynamic response, making it suitable for applications such as robotic joints and mobile robots.
3. Precise Control: Meeting the Requirements of Coordinated Multi-Wheel Motion
Mars Rovers not only need to “move,” but also need to “move precisely.”
CubeMars motors support multiple control methods, including:
Position control
Speed control
Torque control
MIT control mode
At the same time, high-precision encoders are integrated to achieve real-time motion feedback.
For a six-wheel Mars Rover, precise feedback can help:
Synchronize wheel speeds
Improve obstacle-crossing capability
Reduce slippage
Improve motion stability
CubeMars Powers the RoboTeam Twente Mars Rover
Introduction to the RoboTeam Twente Mars Rover Project
To develop a Mars Rover capable of adapting to complex terrain, RoboTeam Twente selected CubeMars motors as its robotic drive solution.
RoboTeam Twente is an interdisciplinary student robotics team from the Netherlands, consisting of students from the University of Twente and Saxion University of Applied Sciences. The team members cover multiple fields, including mechanical design, electronic systems, embedded control, software development, and artificial intelligence. The team is dedicated to developing advanced robotic systems and participating in international Rover competitions.
In the Mars Rover project, the robot needs to complete challenges similar to those encountered in real planetary exploration missions, including:
Complex terrain movement
Autonomous navigation
Environmental exploration
Robot task execution
Therefore, the drive system needs to simultaneously provide:
High torque output
Compact structure
Stable control
Long-term operational reliability
These requirements make the selection of motors and actuators a key part of project development.
Different Reduction Ratio Actuator Combinations for Balancing Power and Response
During operation, the Mars Rover's different motion requirements place different demands on the drive system.
For example, when facing:
- Slope climbing
- Soft ground
Gravel obstacles
and other situations, the robot needs stronger output torque;
While when performing:
- Speed adjustment
- Precise motion control
Coordinated multi-wheel operation
tasks, better dynamic response capability is required.
Therefore, RoboTeam Twente adopted a combination of CubeMars actuators with different reduction ratios to achieve a balance between power and flexibility according to different performance requirements.
AK45-36 KV80: Providing a High Reduction Ratio and Strong Output Capability
CubeMars AK45-36 KV80 adopts a 36:1 reduction ratio design.
A higher reduction ratio can effectively increase output torque, giving the robot stronger low-speed driving capability and load-bearing capability.
For the Mars Rover, when operating in complex environments, the vehicle needs to overcome:
- Ground resistance
- Slope loads
Obstacle impacts
Therefore, high torque output is very important for improving the robot's traversability.
The characteristics of the AK45-36 KV80 make it suitable for drive scenarios that require strong power output, providing stable and reliable motion support for the Rover.
AK70-10 KV100: Balancing Power Output and Dynamic Response
CubeMars AK70-10 KV100 adopts a 10:1 reduction ratio design.
Compared with higher reduction ratio solutions, a lower reduction ratio can provide:
- Faster response speed
- More flexible motion control
Better dynamic performance
For mobile robots, not every scenario requires maximum torque.
In applications that require rapid adjustment of the motion state and greater control flexibility, the AK70-10 KV100 can provide better dynamic performance.
Project video:
Why Does RoboTeam Twente Choose CubeMars Motors?
1. High Torque Output Meets the Requirements of Complex Terrain Movement
During operation, the Mars Rover needs to face:
Sand
Gravel
Slopes
Uneven ground
Compared with ordinary mobile robots, the Rover places higher demands on wheel-end power.
CubeMars AK Series actuators combine brushless motors with planetary reduction structures, helping mobile robots obtain stronger driving force through higher output torque while maintaining a compact size.
For Rover projects, this high torque density design can help the robot achieve stronger motion capabilities within limited space.
2. Highly Integrated Design Reduces System Development Difficulty
Traditional robotic drive solutions usually require separate selection of:
Motor
Reducer
Encoder
Driver
Then mechanical and control matching is carried out.
For student robotics teams or research projects, this increases:
Mechanical design workload
Debugging time
System integration difficulty
CubeMars robotic actuators integrate core motion components, including:
Brushless motor
Reduction mechanism
Encoder
Drive control
Providing a more modular power solution.
This design can help the team focus more on:
Rover structural design
Control algorithm development
Autonomous navigation systems
Instead of spending a great deal of time solving basic drive integration problems.
3. Precise Control Improves Rover Motion Stability
Mars Rovers typically use multiple drive wheels for coordinated motion.
In complex environments, the robot needs to adjust in real time:
Wheel speed
Output torque
Motion state
CubeMars actuators support closed-loop control and provide real-time motion information through encoder feedback, enabling the control system to achieve more precise motion management.
This is very important for Rovers that need to complete complex terrain tasks.
What Types of Robots Are CubeMars Drive Solutions Suitable For?
In addition to Mars Rovers, CubeMars motors and actuators are also suitable for:
1. Mobile Robots
For example:
UGVs
Inspection robots
Outdoor robots
2. Industrial Robots
For example:
AGVs
Automation equipment
Intelligent logistics robots
3. High-Performance Robots
For example:
Humanoid robots
Quadruped robots
Robotic arms
How to Choose the Right Motor for Your Mars Rover?
When selecting a Mars Rover Motor, you can follow the steps below:
1. Determine the Robot Weight
Including:
Vehicle body
Battery
Payload
Mechanical structure
2. Determine the Wheel Parameters
Including:
Wheel diameter
Tire type
Contact area
3. Calculate the Required Torque
Consider:
Maximum slope
Ground resistance
Maximum load
4. Match the Reduction Ratio
According to:
Speed requirements
Torque requirements
Dynamic response
Select the appropriate solution.
5. Confirm the Control Requirements
Select:
Speed control
Position control
Torque control
Conclusion
Mars Rover motor selection is not simply about finding a motor with the maximum torque, but about finding the best balance between power performance, structural size, weight, control precision, and overall system reliability.
For complex mobile robots such as Mars Rovers, the drive system not only determines whether the robot can move, but also affects its traversability, stability, and overall performance in real mission environments.
CubeMars has developed highly integrated motion control solutions for robotic applications by combining:
High-performance brushless motors
Planetary reduction mechanisms
Encoder feedback
Flexible control methods
Providing reliable power support for Mars Rovers, UGVs, mobile robots, and other intelligent robotic platforms.
The application of the RoboTeam Twente Mars Rover project demonstrates the practical value of the CubeMars drive solution in the field of robotic exploration. For teams developing projects involving Mars Rovers, lunar rovers, unmanned mobile platforms, or research robots, selecting suitable robotic motors and actuator solutions is an important step toward improving system performance and shortening the development cycle.
In the future, as robotics technology continues to develop, high-performance, highly integrated, and easy-to-deploy drive systems will play an increasingly important role in planetary exploration, industrial automation, and autonomous mobile robotics.
CubeMars is committed to providing reliable power solutions for robot developers worldwide, enabling robots to achieve stronger motion and exploration capabilities.