Cubemars - 17 Year Motor Manufacturer info@cubemars.com +86 13755649079
English
English
中文简体
日本語
Deutsch
Français
한국어
Español
Pусский
Quick Registration
Create your CubeMars account

 

Moment
TABLE OF CONTENTS
Torque requirements
Speed requirements
Power supply
Motor type
Control system
Size and weight

How to choose motor for robotic

CubeMars / Sep 06,2023

When selecting a motor for a robot application, it is first necessary to determine the operating environment of the robot, which scenarios are mainly used, and which specific actions and tasks need to be done, and then according to the above situation, the following 6 factors should be considered comprehensively:


Torque requirements


Determine the amount of torque needed to perform the desired tasks. This mainly depend on the weight and size of the robot, as well as the tasks it needs to accomplish.


Speed requirements


Because different motors have different speed capabilities, it is particularly important to choose one that meets the speed requirements based on the speed at which the robot needs to move.


Power supply


Determine the available power supply for the robot. This will help you choose a motor that can operate within the given voltage and current limits.


Motor type


There are many types of motors, such as DC motors, servo motors and so on. Each has its own advantages and disadvantages. Combining the application scenarios of your robot, choosing the most suitable robot motor is the top priority.


Control system


Consider the control system you plan to use for the robot. Some motors require specific control mechanisms, so ensure compatibility between the motor and control system.


Size and weight


The size and weight of the motor affect the robot's actions. Therefore, it is important to choose a motor that fits within the available space and is lightweight enough to not hinder the robot's movement.


By considering these factors, you can make an informed decision when choosing a motor for your robotic application.


Related Articles
How do exoskeleton actuators balance power density and human safety?
How do exoskeleton actuators balance power density and human safety?
Focusing on exoskeleton actuator technology, this article analyzes the balance between high power density and human safety, covering human-machine collaboration, compliant control, as well as rehabilitation and industrial applications and selection.
May 07,2026
CubeMars Robotic Actuator Powering Georgia Tech's AI Exoskeletons Featured In Science Advances
CubeMars Robotic Actuator Powering Georgia Tech's AI Exoskeletons Featured In Science Advances
AK80-9 robotic actuators power Georgia Tech's AI exoskeletons, achieving 86% energy efficiency improvement and real-time terrain adaptation for enhanced mobility.
Jul 19,2025
Toronto MetRobotics Achieves Second-Highest Canadian Ranking at University Rover Challenge
Toronto MetRobotics Achieves Second-Highest Canadian Ranking at University Rover Challenge
Toronto MetRobotics (TMR) is a multidisciplinary robotics collective based at Toronto Metropolitan University, comprising students from various faculties united in designing, developing, and manufacturing competitive robots.
Jul 11,2024
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt