Project Background
Research Methodology
1.Real-Time Motion Data Mapping
2.Feedback Force Control
Key Experimental Results
Significance and Future Directions

Bipedal Robot Teleoperation and Dynamic Motion Synchronization Research

CubeMars / Oct 17,2024

Bipedal robots have garnered significant attention in current robotics technology due to their ability to navigate complex environments with agility. As technological advancements continue, researchers are dedicated to developing bipedal robots that can efficiently synchronize with human operators, particularly in applications related to emergencies caused by natural disasters or human-made hazards.


Bipedal Robot


Project Background


Despite notable progress in artificial intelligence, existing bipedal robots still struggle to match human capabilities in motion control and flexibility. To enhance the performance of robots in complex and uncertain environments, a research team proposed a teleoperation system based on bilateral feedback. This system aims to map the human operator's motor intelligence in real-time to the robot, enabling the robot to mimic the operator's gait, jumps, and other dynamic actions.


Research Methodology


In this project, researchers adopted a whole-body teleoperation approach, allowing operators to interact with the robot through wearable devices. The operator's movements are captured by sensors and converted into commands understandable by the robot. To ensure the robot can perform tasks efficiently, the research team designed a bilateral feedback mechanism consisting of two main components:


1.Real-Time Motion Data Mapping


The operator's movement data is scaled in real-time to fit the robot's required proportions, ensuring that the robot can appropriately respond to the operator's actions.


2.Feedback Force Control


While the robot executes movements, feedback forces are provided to help the operator perceive the synchronization level between the robot and their own motions. This enables the operator to adjust based on the robot's speed and status, facilitating smoother collaboration.


Key Experimental Results


During the experimental phase, the robot successfully performed various dynamic actions, including walking, stepping in place, and consecutive jumps. The research team also demonstrated how the robot, under the operator's control, could maintain dynamic balance and adapt to external disturbances. These experiments not only validated the effectiveness of the bilateral feedback mechanism but also provided crucial support for the robot's stability in real-world applications.


Significance and Future Directions


This research highlights the potential of combining human motor intelligence with robotic control, offering new insights for enhancing bipedal robots' capabilities in practical applications. By leveraging this approach, robots can better adapt to complex environments, particularly in emergencies, providing effective support to first responders.


Bipedal Robot


Looking ahead, the research team plans to further optimize control algorithms to improve the robot's flexibility and response speed, enabling it to tackle more complex tasks. This project not only advances the development of bipedal robot technology but also lays the groundwork for closer collaboration between humans and robots.


Related Articles
How to Use CubeMars Actuators
How to Use CubeMars Actuators
CubeMars actuators integrate motor, drive & control. This guide covers selection, applications, AK/AKE series tutorials, firmware flashing & calibration.
Apr 23,2026
CubeMars is honored to be a prominent sponsor of ROBOCON 2024, jointly creating the future of robotics technology.
CubeMars is honored to be a prominent sponsor of ROBOCON 2024, jointly creating the future of robotics technology.
Shenzhen, China, January 24th — In order to support the vigorous development of China's robotics technology industry and cultivate a new generation of young engineers, CubeMars will attend the National Un
Jan 30,2024
Nepali Student Team Develops Low-Cost Ankle-Foot Prosthesis Prototype Using CubeMars AK60-6 Motor
Nepali Student Team Develops Low-Cost Ankle-Foot Prosthesis Prototype Using CubeMars AK60-6 Motor
Recently, a team of Nepali students successfully developed an ankle-foot prosthesis prototype based on the CubeMars AK60-6 motor and subjected it to rigorous testing.
Mar 25,2025
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt