Video Center
TABLE OF CONTENTS
Project Challenge: The "Visual Blind Spot" and "Terrain Dilemma" of Traditional Agricultural Inspection
The Solution: How CubeMars Actuators Empower the "Farmland Explorer"
Video Highlights: Inside the Field with True 3D Crop Inspection
Frequently Asked Questions (FAQ)
Explore More Agricultural and Special Robotics Drive Solutions

CubeMars Powers the University of Minnesota's Agricultural Quadruped Robot Dog

CubeMars / Jul 06,2026

In today's rapidly evolving era of precision agriculture, obtaining comprehensive, high-accuracy crop growth data has become a critical challenge. In this video, we showcase a groundbreaking achievement from the University of Minnesota—an agricultural quadruped robot specifically designed for complex farmland environments.

 

The robot is powered by the CubeMars AK70-10 as its core drive system. By overcoming the physical limitations of traditional drones and wheeled agricultural machines, it can navigate deep into dense cornfields and collect precise pest, disease, and nutrient data beneath the crop canopy, filling a crucial gap in modern smart agriculture with true 3D field inspection.

 

Project Challenge: The "Visual Blind Spot" and "Terrain Dilemma" of Traditional Agricultural Inspection


Although agricultural drones and autonomous tractors have become increasingly common, researchers still face major challenges when monitoring tall crops such as corn and sorghum:


  1. The Inaccessible Area Beneath the Canopy: Drones can only fly above the crop canopy and cannot detect early signs of pests and diseases hidden on the underside of leaves or near the base of stems. Large agricultural machines are simply too bulky to enter dense fields during the middle and late growth stages.

  2. Harsh Unstructured Terrain: Farmland is filled with mud, furrows, weeds, and uneven ground. Traditional wheeled robots can easily become stuck or tip over, making them poorly suited for such complex unstructured environments.

  3. Balancing Payload, Endurance, and Mobilit: The quadruped robot must carry sensors such as multispectral cameras and LiDAR while maneuvering through narrow crop rows. This places extremely demanding requirements on the actuator's power density (torque-to-weight ratio).


The Solution: How CubeMars Actuators Empower the "Farmland Explorer"


To enable the quadruped robot to move across challenging farmland with ease, the University of Minnesota team selected high-performance CubeMars joint actuators. Their key advantages in agricultural robotics include:


  1. Ultra-Compact and Lightweight Design for Narrow Crop Rows: Space inside the robot's legs is limited, and overall weight directly affects how deeply the robot sinks into soft soil. The CubeMars AK70-10 highly integrates a brushless motor, precision gearbox, and driver into a compact, lightweight package. This high-power-density design significantly reduces the robot's weight, allowing it to move through narrow crop rows without damaging plants.

  2. Powerful Torque Output for Mud and Rough Terrain: When crossing furrows or walking through mud, the robot's leg joints must generate large bursts of torque to support the body and pull its feet out of soft ground. CubeMars actuators provide excellent peak torque and overload capability. Combined with advanced FOC control algorithms, they can adjust the torque output of each leg in real time, ensuring stable posture and strong traction on complex terrain.

  3. Industrial-Grade Reliability for Harsh Outdoor Conditions: Farmland environments involve high humidity, dust, intense vibration, and large temperature variations. CubeMars power modules feature industrial-grade sealing and reinforced structural design, offering excellent resistance to dust, water, and vibration. This ensures high stability and long service life during continuous outdoor operation.


Video Highlights: Inside the Field with True 3D Crop Inspection


In this video, you'll see the University of Minnesota agricultural quadruped robot powered by CubeMars actuators in action:


  • Under-canopy navigation: Watch the robot move through dense cornfields while its sensors scan the underside of leaves and the base of stems.

  • Complex terrain traversal: See the robot smoothly cross furrows and avoid weeds, demonstrating outstanding terrain adaptability.

  • Research insights: Hear the University of Minnesota team explain how quadruped robots complement drones by eliminating aerial blind spots, enabling earlier pest and disease detection and more accurate yield estimation.


Frequently Asked Questions (FAQ)


Q1: What irreplaceable advantages do quadruped robots have over agricultural drones in crop monitoring?


A: The greatest advantage is complementary perspective. Drones can only capture data from the top of the crop canopy, while quadruped robots can enter the crop interior and collect high-resolution images and environmental data below the canopy. This is invaluable for detecting pests hidden on leaf undersides, monitoring diseases near the stem base, and assessing the soil microenvironment. Combining drones and quadruped robots enables truly 3D precision agriculture.


Q2: What special challenges do outdoor farmland environments pose for robotic joint actuators?


A: Farmland is far harsher than laboratories or urban roads. Actuators must withstand mud, water splashes, and dust intrusion (requiring high protection ratings), as well as high-frequency impacts and intense vibration during walking (requiring high mechanical strength and vibration resistance). In addition, soft soil demands extremely high instantaneous torque to prevent the robot from getting stuck. CubeMars industrial-grade power modules are specifically designed to meet these demanding requirements.


Explore More Agricultural and Special Robotics Drive Solutions


Whether for agricultural inspection quadrupeds, orchard harvesting robots, or specialized forestry and mining platforms, CubeMars provides high-power-density, high-reliability miniature drive solutions for next-generation field robotics.


[Learn more about the CubeMars AK70-10, including detailed specifications and dimensions]

Related Articles
Tutorial: Setup CubeMars AK60-6 (KV80) for MIT Mode in C++
Tutorial: Setup CubeMars AK60-6 (KV80) for MIT Mode in C++
Learn how to configure the CubeMars AK60-6 (KV80) motor for MIT mode using C++. A step-by-step guide to mastering low-latency position, velocity, and torque control.
Jul 03,2026
KLEIYN Quadruped Wall-Climbing Robot Powered by CubeMars
KLEIYN Quadruped Wall-Climbing Robot Powered by CubeMars
See how the KLEIYN robot uses CubeMars motors and an active waist joint to master wall climbing via reinforcement learning (RL) and CGCL, achieving 150mm/s on narrow walls.
Jun 18,2026
Your Next Robotics Actuator Is Here in CubeMars
Your Next Robotics Actuator Is Here in CubeMars
Maybe you’re interested in CubeMars products, but haven’t had the chance to really get to know who we are. This video will take you inside CubeMars
Aug 29,2025
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt