Cubemars - 17 Year Motor Manufacturer info@cubemars.com +86 13755649079
English
English
中文简体
日本語
Deutsch
Français
한국어
Español
Pусский
Quick Registration
Create your CubeMars account

 

Moment
TABLE OF CONTENTS
Design Concept of LORIS
Mechanical Design and Technical Features
Research and Development

A Case Study for Robotics Enthusiasts: The Climbing Robot LORIS

CubeMars / Aug 01,2024

The Climbing Robot LORIS

In the field of robotics, each new breakthrough sparks limitless creativity and imagination. Today, we delve into a revolutionary quadrupedal climbing robot developed by Carnegie Mellon University (CMU) — LORIS (Lightweight Observation Robot for Irregular Slopes). For robotics enthusiasts, this robot is an exciting case study, demonstrating how future robots can interact with and navigate complex environments.


Design Concept of LORIS


The design of LORIS is inspired by insects and reptiles in nature. These creatures exhibit exceptional climbing abilities on irregular surfaces, inspiring researchers to develop a robot capable of similar feats. Each leg of LORIS is equipped with microspine grippers that can latch onto rocks, bark, and other irregular surfaces, enabling the robot to move freely in complex terrain.


Mechanical Design and Technical Features


LORIS’s uniqueness lies in its microspine grippers. Each gripper consists of multiple tiny hooks that can catch onto small protrusions and indentations, providing strong grip strength. This design not only allows LORIS to climb steep rock faces but also to traverse environments inaccessible to other robots.


Additionally, LORIS is equipped with a depth-sensing camera and an intelligent microprocessor, enabling it to sense its environment in real-time and adjust each leg's movement accordingly. Through complex algorithms, LORIS can intelligently plan each step, maintaining balance and ensuring stable grip.


Research and Development


The development of LORIS is the result of the dedicated efforts of the team at CMU’s Robomechanics Lab. The team, consisting of researchers like Paul Nadan, Spencer Backus, and Aaron M. Johnson, succeeded in creating a robot that can freely climb irregular slopes through continuous experimentation and optimization.

To achieve this, researchers employed a technique called Directed Inward Grasping (DIG). This technique, inspired by insect climbing methods, involves the grippers closing inward to secure the surface, providing stable support. LORIS’s design is not only lightweight and efficient but also achieves an ideal balance between energy consumption and movement speed.


Conclusion

LORIS is not only a significant breakthrough in robotics but also a case study worthy of attention and learning for robotics enthusiasts. It demonstrates how inspiration from nature can be transformed into engineering design and how innovative technology can achieve outstanding performance. This research by CMU provides valuable experience and insights for the future development of robotics, inspiring more individuals to engage in this promising field.


For further reference:

1.CMU Robomechanics Laboratory

2.Robotics and Automation

3.Nature-Inspired Robotics


Related Articles
Complex Environment Robot Motor Applications: From Space Exploration and Extraterrestrial Missions to Long-Term Unmanned Operation
Complex Environment Robot Motor Applications: From Space Exploration and Extraterrestrial Missions to Long-Term Unmanned...
Motor selection for robots operating in complex environments should not focus solely on individual parameters such as peak torque and speed. Instead, it requires a comprehensive evaluation based on the actual operating conditions, robotic tasks, mechanica
Sep 28,2026
Which motors are used for walking robots
Which motors are used for walking robots
Walking robots typically use a combination of different types of motors to achieve locomotion. The specific motors used can vary depending on the design and requirements of the robot.
Sep 06,2023
CubeMars Sponsors Binghamton University Robotics Team for the 2024 University Rover Challenge (URC)
CubeMars Sponsors Binghamton University Robotics Team for the 2024 University Rover Challenge (URC)
CubeMars is thrilled to announce our sponsorship of the Binghamton University Robotics Team for their participation in the 2024 University Rover Challenge (URC), hosted by the National Aeronautics and Space Administration (NASA). URC is an international r
May 08,2024
Leave Message
User name
Anonymous
E-mail *
Name *
Phone
Comments
Verification code
captcha
Warm prompt
Warm prompt
Please Sign In
Sign In
Sign Up
Forgot Password?
Warm prompt